Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Cross Compiling for Ubuntu and Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 796 views
  • Users 0 members are here
Related

Cross Compiling for Ubuntu and Zedboard

100badrobit
100badrobit over 9 years ago

I am working with an application written in C++ that I have compiling and running on Ubuntu 16.04.2 and I want to add something that will let me compile and run the application on our Zedboard. I try to use CMake where possible and I have created this toolchain file: 

# This is a CMAKE file used to describe the toolchain required

# for cross compiling for the Zedboard with the Zynq 7020.
 
# TODO: find a better way to do this.
include(CMakeForceCompiler)
 
# Provide a system name and path to the compilers.
set(CMAKE_SYSTEM_NAME Linux)
set(CMAKE_C_COMPILER arm-linux-gnueabi-gcc)
set(CMAKE_CXX_COMPILER arm-linux-gnueabi-g++)
 
# Set the root directory for the ARM toolchain
set(CMAKE_FIND_ROOT_PATH "/usr/arm-linux-gnueabi")
 
# Set how the root path should be used.
set(CMAKE_FIND_ROOT_PATH_MODE_PROGRAM NEVER)
set(CMAKE_FIND_ROOT_PATH_MODE_LIBRARY ONLY)
set(CMAKE_FIND_ROOT_PATH_MODE_INCLUDE ONLY)
set(CMAKE_FIND_ROOT_PATH_MODE_PACKAGE ONLY)
 
The goal is to allow for faster development to build the program and copy it over to the Zedboard and run it as an application. When I build the program and link it I have no issues. I then copy it over to the Zedboard and try to run it using ./app and I get the following error: 
 
  -sh: ./app: No such file or directory
   
  I am hoping someone can point me to where I am doing something incorrect. I have added the CMake file I use to generate the make files below: 
   
 
   cmake_minimum_required(VERSION 3.0)
 
   project("App")
 
    
 
   add_executable( app "app.cpp" )
   
 
  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 9 years ago

    Hi badrobit,

    Ubuntu is a pretty fully featured version of Linux and we typically don't see that getting run on ZedBoard.

    Which version of Linux are you running on ZedBoard?

    Regards,

    -Kevin