Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development AXI_CDMA driver of linux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 329 views
  • Users 0 members are here
Related

AXI_CDMA driver of linux

zxj
zxj over 11 years ago

I want to test AXI_CDMA driver of linux, and do like
this Link:

http://www.wiki.xilinx.com/DMA+Drivers+-+Soft+IPs

Step1:
    config the kernel:

    CONFIG_XILINX_AXICDMA=Y
    CONFIG_XILINX_CDMATEST=Y

Step2:
    add device in zynq_zed.dts

    axi_cdma_0: axicdma@40030000 {
    compatible = "xlnx,axi-cdma";
    reg = < 0x40030000 0x10000 >;
    dma-channel@40030000 {
        interrupts = < 0 59 4 >;
        xlnx,datawidth = <0x40>;
        xlnx,device-id = <0x0>;
    } ;
} ;

and then conpile kernel, the boot message :

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
Booting Linux on physical CPU 0x0
Linux version 3.12.0-xilinx-dirty (root@ubuntu) (gcc version 4.7.3 (Sourcery CodeBench Lite 2013.05-40) ) #158 SMP PREEMPT Mon Jan 26 18:43:01 PST 2015
CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Xilinx Zynq Platform, model: Xilinx Zynq
bootconsole [earlycon0] enabled
Memory policy: Data cache writealloc
PERCPU: Embedded 8 pages/cpu @c09ef000 s8384 r8192 d16192 u32768
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 121856
Kernel command line: console=ttyPS0,115200 root=/dev/ram rw earlyprintk
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 476800K/491520K available (4106K kernel code, 246K rwdata, 1304K rodata, 176K init, 175K bss, 14720K reserved, 0K highmem)
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    vmalloc : 0xe0800000 - 0xff000000   ( 488 MB)
    lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    modules : 0xbf000000 - 0xbfe00000   (  14 MB)
      .text : 0xc0008000 - 0xc0550c58   (5412 kB)
      .init : 0xc0551000 - 0xc057d0c0   ( 177 kB)
      .data : 0xc057e000 - 0xc05bbbc8   ( 247 kB)
       .bss : 0xc05bbbd4 - 0xc05e79e8   ( 176 kB)
Preemptible hierarchical RCU implementation.
        Dump stacks of tasks blocking RCU-preempt GP.
        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
NR_IRQS:16 nr_irqs:16 16
ps7-slcr mapped to e0802000
Zynq clock init
sched_clock: 16 bits at 54kHz, resolution 18432ns, wraps every 1207ms
ps7-ttc #0 at e0804000, irq=43
Console: colour dummy device 80x30
Calibrating delay loop... 1332.01 BogoMIPS (lpj=6660096)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0xc03e2ac0 - 0xc03e2b18
L310 cache controller enabled
l2x0: 8 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x72360000, Cache size: 512 kB
CPU1: Booted secondary processor
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
Brought up 2 CPUs
SMP: Total of 2 processors activated.
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
zynq_gpio e000a000.ps7-gpio: gpio at 0xe000a000 mapped to 0xe0850000
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
zynq_ocm f800c000.ps7-ocmc: ZYNQ OCM pool: 256 KiB @ 0xe0880000
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
EDAC MC: Ver: 3.0.0
Switched to clocksource ttc_clocksource
NET: Registered protocol family 2
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP: reno registered
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (no cpio magic); looks like an initrd
Freeing initrd memory: 4296K (df71f000 - dfb51000)
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
jffs2: version 2.2. (NAND) (SUMMARY)  ?? 2001-2006 Red Hat, Inc.
msgmni has been set to 939
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
dma-pl330 f8003000.ps7-dma: unable to set the seg size
dma-pl330 f8003000.ps7-dma: Loaded driver for PL330 DMAC-2364208
dma-pl330 f8003000.ps7-dma:     DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16
---- xilinx_cdma_probe start!----


And the linux system freezes!!!
What's wrong please?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    This behavior is typical when the driver requests information from the hardware, but never gets a response.  There are many reasons why this could happen, but they all boil down to a disconnect in the communications path between the hardware platform and the OS driver.  First thing to check is that the hardware platform has been built correctly.  Have you run all the self-tests for the soft IP in your system?  Validating the hw platfrm without an OS is the first step.  If the hw checks out, then we can look at the likely areas in the software.

    Ron