Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Embedded Vision Demo won't run
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 968 views
  • Users 0 members are here
Related

Embedded Vision Demo won't run

thosch42
thosch42 over 11 years ago

Hi all!

My Embedded Vision Development Kit with Python-1300 camera module just arrived and I'm doing my first steps.

First of all, I saved the sd image from the Getting Started Guide to the sd card and run the kit from this image. Everything works fine.
Then I followed the steps described in the PYTHON-1300-C Reference Design pdf. The build of the design works well and the Synthesis as well as the Implementation runs without errors. Even the Compilation of the embedded software project in the SDK run without errors. So far, so good.
But when I program the FPGA and run the application, I get nothing. So it seems, that the provided sd-image and the result of the build process of the provided Reference Design is not the same.
So the question is, where did I get the right Reference Design?

Best regards,
Thomas

  • Sign in to reply
  • Cancel
Parents
  • albertabeef
    0 albertabeef over 11 years ago

    Thomas,

    I will help you to get this design working.

    The design was built and tested on hardware before being posted online.  I will re-download, re-build, and re-test the design as an additional verification step.

    In the meantime, can you confirm if the pre-built BOOT.bin that is included with the design works ? (C:\AVNET_EMBV_PYTHON1300\2014_3\sd_image\microzed_7020\BOOT.bin)

    Also, can you provide the output of the serial console ?  This can provide additional clues to help resolution of this issue.

    Regards,

    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • albertabeef
    0 albertabeef over 11 years ago

    Thomas,

    I will help you to get this design working.

    The design was built and tested on hardware before being posted online.  I will re-download, re-build, and re-test the design as an additional verification step.

    In the meantime, can you confirm if the pre-built BOOT.bin that is included with the design works ? (C:\AVNET_EMBV_PYTHON1300\2014_3\sd_image\microzed_7020\BOOT.bin)

    Also, can you provide the output of the serial console ?  This can provide additional clues to help resolution of this issue.

    Regards,

    Mario.