Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development AXI DMA7.1 Cyclic mode problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 802 views
  • Users 0 members are here
Related

AXI DMA7.1 Cyclic mode problem

e14 Contributor
e14 Contributor over 12 years ago

Hi,
I'm using a reference design that includes an Analog to Digital Converter (ADC) connected to the FMC connector,AXI DMAand DDR3 Ram on ZEDBOARD.I want transfer the  data from AD to DDR via AXI DMA continuously.

Now I use ISE 14.7,the lastest vertion of AXI DMA is 6.03a,it doesn't support cyclic BD mode .I know the lastest vertion of DMA in VIVADO is 7.1,it support cyclic BD mode. So I copy the VIVADO'S DMA IP(v7.1) to ISE14.7, I use it in xps like blow my attachment.

1)u3001The first question, can I copy he vivado's DMA IP(v7.1) to ISE14.7,  the DMA IP(v7.1)  is All applicable in VIVADO and ISE?

I use the DMA SG mode ,Program the DMA IP driver in linux, I allocate buffer for DMA, and connect the buffer in Circular buffer.
The Built-in DMA driver in linux xilinx_axidma.c ,I modify it to enable cyclic BD mode like blow  my attachment.

2)u3001My second question ,The Built-in DMA driver xilinx_axidma.c in linux-xlnx-xilinx-v2013.4,have  xilinx_axidma.c modified to support cyclic BD mode?

if  the above two question is YES. I test the  DMA transfer ,However,when data transfered to the last buffer descriptor ,The s_axis_s2mm_sts_tready  signal  at AXI DMA interface pulled down ,then the DMA suspend transmission.

3)u3001Third question , Why the s_axis_s2mm_sts_tready  signal  at AXI DMA interface pulled down? Should it  run forever in cyclic mode ?

Any insight will be appreciated!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The attachement is here http://forums.xilinx.com/t5/Embedded-Linux/AXI-DMA7-1-Cyclic-mode-problem/td-p/511949

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The attachement is here http://forums.xilinx.com/t5/Embedded-Linux/AXI-DMA7-1-Cyclic-mode-problem/td-p/511949