Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development TrustZone
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 364 subscribers
  • Views 1186 views
  • Users 0 members are here
Related

TrustZone

e14 Contributor
e14 Contributor over 13 years ago

Hey all,

does anyone know where to find a tutorial of how to implement TrustZone on the Zynq device?

I have found the TrustZone Spec and the API but I don't know how to use it.

I'm looking for a "Hello World" like a secure UART (or similar) that I can only use in secure world but not in normal world. (or a similar program).
It would be great if it also includes the changes at hardware site.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hey all,

    I was just wondering if no one is working with TrustZone! At least I figured out what's about the TZAPI but I'm still missing the TZ monitor.
    Therefore now the question: Does anyone of you knows how to implement the TrustZone Monitor to switch from secure to normal world?

    br
    schlauby

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    hi,schlauby! I am a student from China using ZedBoard to develop trustzone applications. I meet almost the same program with you, I ran a secure program suceess on zedboard, But when switch to non-secure world, it crashed with no uart output , but i found the non-secure world program is running to some where bugged, and also found i have to configure the TZPC and TZASC,TZMA, and this is controlled by the SCLR . But I found nothing about this registers in ZYNQ MANNUL UG585. So do you find how to configure it , we can discuss using email ,my email address is fanghuaqi@vip.qq.com . Best Wishes!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Can someone post "Hello Secure/Normal World" example of TrustZone software similar to

    http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.faqs/ka15417.html

    but for Xilinx SDK & ZedBoard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Hey all,

    I forgott to write in this forum as well, after writing my solution in the xilinx forum.

    My problem was regarded to the TZ_OCM_RAM0 register. Before starting the secure code we should set the TZ_OCM_RAM0 regarding to our scattering file.
    With this register we can set blocks of the OCM to either secure or non-secure. If all blocks are set to secure (default) we cannot run the non-secure world.

    Each bit in the register represents the TrustZone status for a 4 KB page. (0: Secure, 1: Non-Secure)

    I hope this information will help some of you.

    br
    Schlauby

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi Schlauby,

    I was wondering how you found the address of the TZ_OCM_RAM0 register? Like Fanghuaqi, I am using the Zynq TRM as a reference. I'm seeing a lot of coprocessor 15 commands, but no direct register access.

    Could you maybe post some Xil_Out32 calls or some assembler that you used to set these registers?

    TIA.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi Mark,

    The closest thing I've found is xapp 1079, "bare metal AMP", and making a custom peripheral.

    http://www.microzed.org/content/how-run-two-different-task-parallely-two-standalone-processors-zedboard

    If you go into the HDL and MPD files, S_AXI_AWPROT and S_AXI_ARPROT are both std_logic_vector[2:0], and bit 1 will show you whether you are in secure world. The AXI4_Lite handler won't do stuff automatically but you can change your user_logic.vhd . The AXI bus controller though does support AxPROT.

    So if you read/write to/from a custom peripheral, and set it up with an IRQ, then you should be able to get the same functionality.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    On page 686 of my book, Chapter 29 "On Chip Memory" part 3 "Register Overview", I do see TZ_OCM_RAM0 . But when I look for the actual address in Appendix B "Register Details" section 28 "System Level Control Registers", page 1493, I can't find it anywhere in the table, even though I see the other registers there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    So I tried just setting every unknown TrustZone register in the SLCR to 0xFFFFFFFF, hoping to hit TZ_OCM_RAM0. And I'm still crashing whenever I try to switch to normal world.

    Code,

    #include <stdio.h>
    #include "TrustZone.h"
    #include "xil_io.h"

    void tz_init()
    {
    tint i;
        /* unlock */
    tfor (i = SCLR_TZ_BASE_OFFSET; i < TZ_DMA_NS_BASE_OFFSET; i += 4)
    ttXil_Out32(i, 0xFFFFFFFF);
        Xil_Out32(TZ_DMA_NS_BASE_OFFSET, 0x00000001);
        Xil_Out32(TZ_DMA_IRQ_NS_BASE_OFFSET, 0x0000FFFF);
        Xil_Out32(TZ_DMA_PERIPH_NS_BASE_OFFSET, 0x0000000F);
    tfor (i = TZ_DMA_PERIPH_NS_BASE_OFFSET; i < SCLR_TZ_BASE_OFFSET + 0x0100; i += 4)
    ttXil_Out32(i, 0xFFFFFFFF);
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lmeilan
    0 lmeilan over 10 years ago

    Hi

    I saw on the Xilinx forum(https://forums.xilinx.com/t5/Embedded-Linux/Creating-a-Trustzone-on-Zynq/td-p/275574) where it was mentioned NDA is required to be signed before trustzone could be implemented? Is the Zedboard affected as well?

    Thanks!

    Rdgs

    Meilan