Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Unable to detect the zedboard as device using usb interface
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 363 subscribers
  • Views 1802 views
  • Users 0 members are here
Related

Unable to detect the zedboard as device using usb interface

e14 Contributor
e14 Contributor over 14 years ago

Hi
I'm using the digilent linux source code and i'm able to use zedboard as host in USB interface. When i try use zedbaord as device then it is not detecting with host PC. I have removed the jumpers J2 & J3 to detect as device. But still it is failing. Could you help us to solve this issue?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    1) Yes

    Also I try to connect android board with the zedboard and observed the same result. It looks that the usb driver of the zedboard is not detecting the host machines when it is in device mode.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    1) Yes

    Also I try to connect android board with the zedboard and observed the same result. It looks that the usb driver of the zedboard is not detecting the host machines when it is in device mode.