Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Microzed Wilink8 BT on Linux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 363 subscribers
  • Views 1228 views
  • Users 0 members are here
Related

Microzed Wilink8 BT on Linux

e14 Contributor
e14 Contributor over 11 years ago

We're having a bit of difficulty getting BT up and running even on the I/O carrier card with the Wilink8.

I've been following this guide: http://microzed.org/sites/default/files/documentations/GSG-AES-PMOD-WILINK8-G-v1_6.pdf

And also the reference design here: http://zedboard.org/support/design/6491/66

However, it appears to only be a ramdisk and even when I dig around into the files I can't seem to find much in the way of an example of bringing up BT.

The closest I have is from the pdf guide, Appendex D:
# Enable the Bluetooth radio by setting the BT_EN pin high echo 54 > /sys/class/gpio/export echo out > /sys/class/gpio/gpio54/direction echo 1 > /sys/class/gpio/gpio54/value # Bluetooth modules (drivers) do not require loading, - they are already built into the kernel # activate BlueZ hciattach -t 30 -s 115200 /dev/ttyPS1 texas 3000000 flow hciconfig

When I get to the hciattach step, it gets stuck with an initialization timeout error.

I think I have the device tree setup correctly and the hardware design from the guides and reference designs. If you could send any more information along (a full linux system with a bt script) or put me in touch with someone to help get this working that would be great, or any ideas on what to look out for in terms of potential problems.

I can post any further information if it will be helpful.

Jason

  • Sign in to reply
  • Cancel
Parents
  • peterfenn
    0 peterfenn over 11 years ago

    The Bluetooth-specific issue with this particular build, was determined to be due to a missing (previously applied) kernel patch that was required to fix a hardware flow-control bug in linux-xlnx/drivers/tty/serial/xilinx_uartps.c.

    Though the serial flow control setting had been enabled in the devicetree, this setting was not being used by the driver.

    This has since been fixed and the repository updated

    Do the following steps to rebuild the corrected uImage Linux kernel image file 

    1. Delete your linux-xlnx folder
    2. Re-execute the provided uz_kernel.sh script file to rebuild your Linux kernel from scratch.
    3. Copy the generated uImage file to the SD card BOOT folder

    ie.
    $ cd ~/Documents
    $ rm -Rf linux-xlnx
    $ ./uz_wl8_kernel.sh
    $ cp ~/Documents/linux-xlnx/arch/arm/boot/uImage /media/BOOT

    Regards
    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • peterfenn
    0 peterfenn over 11 years ago

    The Bluetooth-specific issue with this particular build, was determined to be due to a missing (previously applied) kernel patch that was required to fix a hardware flow-control bug in linux-xlnx/drivers/tty/serial/xilinx_uartps.c.

    Though the serial flow control setting had been enabled in the devicetree, this setting was not being used by the driver.

    This has since been fixed and the repository updated

    Do the following steps to rebuild the corrected uImage Linux kernel image file 

    1. Delete your linux-xlnx folder
    2. Re-execute the provided uz_kernel.sh script file to rebuild your Linux kernel from scratch.
    3. Copy the generated uImage file to the SD card BOOT folder

    ie.
    $ cd ~/Documents
    $ rm -Rf linux-xlnx
    $ ./uz_wl8_kernel.sh
    $ cp ~/Documents/linux-xlnx/arch/arm/boot/uImage /media/BOOT

    Regards
    Peter