Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Microzed Wilink8 BT on Linux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 363 subscribers
  • Views 1223 views
  • Users 0 members are here
Related

Microzed Wilink8 BT on Linux

e14 Contributor
e14 Contributor over 11 years ago

We're having a bit of difficulty getting BT up and running even on the I/O carrier card with the Wilink8.

I've been following this guide: http://microzed.org/sites/default/files/documentations/GSG-AES-PMOD-WILINK8-G-v1_6.pdf

And also the reference design here: http://zedboard.org/support/design/6491/66

However, it appears to only be a ramdisk and even when I dig around into the files I can't seem to find much in the way of an example of bringing up BT.

The closest I have is from the pdf guide, Appendex D:
# Enable the Bluetooth radio by setting the BT_EN pin high echo 54 > /sys/class/gpio/export echo out > /sys/class/gpio/gpio54/direction echo 1 > /sys/class/gpio/gpio54/value # Bluetooth modules (drivers) do not require loading, - they are already built into the kernel # activate BlueZ hciattach -t 30 -s 115200 /dev/ttyPS1 texas 3000000 flow hciconfig

When I get to the hciattach step, it gets stuck with an initialization timeout error.

I think I have the device tree setup correctly and the hardware design from the guides and reference designs. If you could send any more information along (a full linux system with a bt script) or put me in touch with someone to help get this working that would be great, or any ideas on what to look out for in terms of potential problems.

I can post any further information if it will be helpful.

Jason

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    We finally got around to trying with the latest instructions. Works with our kernel and our boards. Thanks for the help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    We finally got around to trying with the latest instructions. Works with our kernel and our boards. Thanks for the help!