Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Configuring Minized Petalinux Wi-Fi with custom PL
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 18 replies
  • Subscribers 367 subscribers
  • Views 4444 views
  • Users 0 members are here
Related

Configuring Minized Petalinux Wi-Fi with custom PL

caheike1
caheike1 over 9 years ago

I programmed my logic into the PL on a minized and using the petalinux tools configured a 4.9 version of petalinux for it.  Linux and the PL work well, except networking.  The wifi.sh script that came with the minized does a ‘modprobe bcmdhd’.   This appears to be a custom kernel module that contains the Wi-Fi drivers.  I am unable to find the source for the module so that I can build it myself  or to configure the kernel to support this Wi-Fi chip without the module.  Also,  I would also like to get a copy of the configuration files for the petalinux kernel and rootfs that matches the image.ub that comes with the board so that I can create my own image.ub using my version of the PL.   Has anyone successfully built a petalinux image.ub and gotten Wi-Fi to work?    Does anyone know where to get the stock petalinux configuration files?

  • Sign in to reply
  • Cancel

Top Replies

  • caheike1
    caheike1 over 9 years ago in reply to stefanrousseau +2
    That’s exactly what I needed. I looked for a the correct BSP on the Xilinx website, and could not find a minized version. I failed to look at the minized reference designs. I am now able to install petalinux…
  • stefanrousseau
    stefanrousseau over 9 years ago +1 verified
    On the MiniZed page ( http://zedboard.org/product/minized ) under Reference Designs you will find the PetaLinux 2017.2 BSP. If you create a new project with petalinux-create -t project -n minized -s MiniZed…
  • stefanrousseau
    stefanrousseau over 9 years ago +1
    If you are having issues with the MiniZed JTAG, you could make sure you are able to program by following the steps in the " Restore QSPI and eMMC Factory Images " document under Documents on the MiniZed…
Parents
  • andycap
    0 andycap over 9 years ago

    An Update:

     

    copying the image.ub via a usb stick and I can boot ok into 4.9.0-xilinx-v2017.2 so it looks like everything is building fine, it is just the transferring over jtag that seems to cause the problem.

     

    A bit stumped here!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • andycap
    0 andycap over 9 years ago

    An Update:

     

    copying the image.ub via a usb stick and I can boot ok into 4.9.0-xilinx-v2017.2 so it looks like everything is building fine, it is just the transferring over jtag that seems to cause the problem.

     

    A bit stumped here!