Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development UART-0 hangs when UART-1 receive data in AMP
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 364 subscribers
  • Views 648 views
  • Users 0 members are here
Related

UART-0 hangs when UART-1 receive data in AMP

fayyazrafiq
fayyazrafiq over 12 years ago

Hi All,

I am using ZEDBoard with AMP application. I configured UART0 receive interrupt for CPU0 and UART1 receive interrupt for CPU1. The program works fine, if I do not have any character receive from UART-1. As soon as, i send some character from the terminal program for UART1, UART0 also stop sending data out. I do not know what is problem, It seems something is shared between the CPU0 and CPU1. Although, it should not be the case because i am using separate UART for each CPU. Any help is highly appreciated.

Regards
Fayyaz

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    You didn't supply enough information to fully frame your question.  I see now this is a different problem, so it needs a different solution.  As you state in your question, this could be a problem with the interrupt reaching the processor, but there are also a number of other possibilities.  The first step is to try to narrow down the problem.  I would suggest setting a breakpoint inside the interrupt handler running on the core where you lose UART traffic - you'll have to be a little clever with when you activate it to avoid having it trip before you want it to.  If it does get hit, the interrupt is not the problem.  If it doesn't, then is the interrupt being generated by the UART correctly?  You should be able to check that with ILA/Chipscope.  If it is generated, and the handler doesn't see it, then it must be masked out, so you'll need to look at the low level interrupt function to see what can be done to make sure you don't miss an interrupt while the first handler instance is servicing.  If you are using your own interrupt mechanism, make sure you aren't spending too long inside the handler.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    You didn't supply enough information to fully frame your question.  I see now this is a different problem, so it needs a different solution.  As you state in your question, this could be a problem with the interrupt reaching the processor, but there are also a number of other possibilities.  The first step is to try to narrow down the problem.  I would suggest setting a breakpoint inside the interrupt handler running on the core where you lose UART traffic - you'll have to be a little clever with when you activate it to avoid having it trip before you want it to.  If it does get hit, the interrupt is not the problem.  If it doesn't, then is the interrupt being generated by the UART correctly?  You should be able to check that with ILA/Chipscope.  If it is generated, and the handler doesn't see it, then it must be masked out, so you'll need to look at the low level interrupt function to see what can be done to make sure you don't miss an interrupt while the first handler instance is servicing.  If you are using your own interrupt mechanism, make sure you aren't spending too long inside the handler.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • fayyazrafiq
    0 fayyazrafiq over 12 years ago in reply to e14 Contributor

    Hi

    Thanks again and sorry for incomplete explanation. If you need more explanation, i can provide you.

    I cannot run the AMP application in debugger because i have to run the both applications (cpuo and cpu1). For info, i am using sdk 14.5. I am using the SD card for this purpose. Could you please suggest me, how can i debug the application and where can i found the notes for xilinx system debugger for debugging both applications simultaneously.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to fayyazrafiq

    Hello Fayyaz,

     

    Take a look at the Xilinx appnote xapp1079. It is a bare metal AMP example on the Zynq and shows how to debug both cores:

     

    http://www.xilinx.com/support/documentation/application_notes/xapp1079-amp-bare-metal-cortex-a9.pdf

     

    -Gary