Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development If I want to use UART0 and UART1, what need I do?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 3932 views
  • Users 0 members are here
Related

If I want to use UART0 and UART1, what need I do?

e14 Contributor
e14 Contributor over 11 years ago

Hi all,
   I can run the linux kernel (provided by ADI) on my custom zedboard, where the output message is come from UART1.However, I hope to use UART1 and UART0 at the same time. I have set the pin of MIO 14 and MIO 15 for uart0 in XPS configuration and enabled the UART0 port. I also glanced over the file of my devicetree.dts  which is correspond with the current devicetree.dtb. In my opnion, the UART0  has been defined correctly in that file.
    Generaly, kernel will print:
----------------------------
e0001000.uart: ttyPS0 at MMIO 0xe0001000 (irq = 82) is a xuartps
console [ttyPS0] enabled
e0000000.uart: ttyPS1 at MMIO 0xe0000000 (irq = 59) is a xuartps
----------------------------
    Unfortunately, I can't find any message about "ttyPS1" from kernel output.
    Has any one can help me or give me any tips??

Thanks!

the following is the part of my dts file about uart , if i remove 'the status = "disabled";', the kernel will be blocked.
--------------------------------------------------
    compatible = "xlnx,zynq-7000";
    #address-cells = <0x1>;
    #size-cells = <0x1>;
    interrupt-parent = <0x1>;
    model = "Xilinx Zynq ZED";

    aliases {
        ethernet0 = "/amba@0/eth@e000b000";
        serial0 = "/amba@0/uart@e0001000";
    };

    chosen {
        bootargs = "console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait";
        linux,stdout-path = "/amba@0/uart@E0001000";
    };

    amba@0 {
        compatible = "simple-bus";
        #address-cells = <0x1>;
        #size-cells = <0x1>;
        ranges;
        linux,phandle = <0x2>;
        phandle = <0x2>;

        .....
        uart@e0000000 {
            compatible = "xlnx,xuartps";
            status = "disabled";
            reg = <0xe0000000 0x1000>;
            interrupts = <0x0 0x1b 0x4>;
            interrupt-parent = <0x1>;
            clock-names = "ref_clk", "aper_clk";
            clocks = <0x3 0x17 0x3 0x28>;
            port-number = <0x0>;
            current-speed = <0x1c200>;
            device_type = "serial";
        };

        uart@e0001000 {
            compatible = "xlnx,xuartps";
            reg = <0xe0001000 0x1000>;
            interrupts = <0x0 0x32 0x4>;
            interrupt-parent = <0x1>;
            clock-names = "ref_clk", "aper_clk";
            clocks = <0x3 0x18 0x3 0x29>;
            port-number = <0x0>;
            current-speed = <0x1c200>;
            device_type = "serial";
        };
}

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 11 years ago

    I'm not sure of the answer, but I found a couple other posts that look relevant. Will you please review and reply if you find something useful here?

     

    https://forums.xilinx.com/t5/Embedded-Linux/Enabling-the-second-UART-on-the-ZC702-Zynq-Dev-Board/td-p/236674

    https://forums.xilinx.com/t5/Embedded-Linux/How-to-call-UART0-quot-ttyPS0-quot-and-UART1-quot-ttyPS1-quot/td-p/518435

    https://forums.xilinx.com/t5/Embedded-Linux/Enabling-a-second-UART-on-ZC706-for-AMP-Linux-Baremetal/td-p/504865

    https://forums.xilinx.com/t5/Embedded-Linux/Zynq-second-UART-no-output-to-minicom/td-p/377621

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 11 years ago

    I'm not sure of the answer, but I found a couple other posts that look relevant. Will you please review and reply if you find something useful here?

     

    https://forums.xilinx.com/t5/Embedded-Linux/Enabling-the-second-UART-on-the-ZC702-Zynq-Dev-Board/td-p/236674

    https://forums.xilinx.com/t5/Embedded-Linux/How-to-call-UART0-quot-ttyPS0-quot-and-UART1-quot-ttyPS1-quot/td-p/518435

    https://forums.xilinx.com/t5/Embedded-Linux/Enabling-a-second-UART-on-ZC706-for-AMP-Linux-Baremetal/td-p/504865

    https://forums.xilinx.com/t5/Embedded-Linux/Zynq-second-UART-no-output-to-minicom/td-p/377621

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to bhfletcher

    hi, Bryan
     
       Thank you for your message!
       I had fixed it by modifying DTS file.
       Thanks!

    Kind Regards,
    Lee