Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development problems compiling dbus-1.6.10
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 353 views
  • Users 0 members are here
Related

problems compiling dbus-1.6.10

e14 Contributor
e14 Contributor over 13 years ago

Hi all,

I need to use Bluetooth i/f, so I need to install Bluez-5.5; to do this I need to install some libraries, one of these is dbus-1.6.10.

I have a problem with configuring dbus (only with dbus);
the folder with the target file system is:
/home/zedboard/rootfs64M

and I use this command:

groupadd -g 18 messagebus &&
useradd -c "D-Bus Message Daemon User" -d /home/zedboard/rootfs64M/var/run/dbus
        -u 18 -g messagebus -s /home/zedboard/rootfs64M/bin/false messagebus
tt
export LDFLAGS=-Wl,-L/home/zedboard/rootfs64M/usr/lib,-lexpat
export CPPFLAGS=-I/home/zedboard/rootfs64M/usr/includett
./configure
--host=arm-xilinx-linux-gnueabi
--prefix=/home/zedboard/rootfs64M/usr
--sysconfdir=/home/zedboard/rootfs64M/etc
--localstatedir=/home/zedboard/rootfs64M/var
--libexecdir=/home/zedboard/rootfs64M/usr/lib/dbus-1.0
--with-console-auth-dir=/home/zedboard/rootfs64M/run/console/
--without-systemdsystemunitdir
--disable-systemd
--disable-static

the result is:
...
checking how to create a ustar tar archive... gnutar
checking whether to enable maintainer-specific portions of Makefiles... yes
checking whether make supports nested variables... yes
checking for gcc... arm-xilinx-linux-gnueabi-gcc
checking whether the C compiler works... no
configure: error: in `/home/zedboard/git_folder/dbus-1.6.10':
configure: error: C compiler cannot create executables
See `config.log' for more details
zedboard:>

and then it stops!

I cannot understand why only for this package the compiler does not work, while with the other packages I do not have any problems

As anyone had and solved this kind of problem?

best regards,
   Roberto

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    the problem is in the configure script at line 4157, where the test expects a result equal to variable "maybe", defined at line 1441, but does not matches;
    --
    the work around I've found consists in modifying line 4157
    from:
        if test "$cross_compiling" = maybe; then
    to:
        if test "$cross_compiling" != 0; then
    --

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    the problem is in the configure script at line 4157, where the test expects a result equal to variable "maybe", defined at line 1441, but does not matches;
    --
    the work around I've found consists in modifying line 4157
    from:
        if test "$cross_compiling" = maybe; then
    to:
        if test "$cross_compiling" != 0; then
    --