Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Load new application on CPU1 while running Linux on CPU0?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 363 subscribers
  • Views 651 views
  • Users 0 members are here
Related

Load new application on CPU1 while running Linux on CPU0?

e14 Contributor
e14 Contributor over 13 years ago

Is there anyone that have an idea how to load a new application (.elf) on CPU1 while running Linux on the other core (CPU0) without rebooting Linux?

I'm using a Zedboard and running simple AMP based on Xilinx XAPP1078.

I have tried to soft-reset the CPU1 but I can't start the application again after reset. Do I have to do anything special after a reset? I have just tried to start the application by writing the start-address to 0xfffffff0.

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 13 years ago

    A ZedBoard port of XAPP1078 is now posted under Reference Designs.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to bhfletcher

    Hello,

    I am trying to utilize both cpu0 and cpu1 on zed board.
    Using the document xapp1078,that document having operation of cpu0 on linux and cpu1 on bare-metal.

    First, I downloaded the following generated files and copied to SD card them.

    http://www.zedboard.org/sites/default/files/design/xapp1078_zedboard.zip,

    <SD card>
    - BOOT.BIN
    - devicetree.dtb
    - uImage
    - uramdisk.image.gz
    - rwmem.elf
    - softUart.elf

    After I switched on Zed Board,booting process has to start, and booting process(cpu0) was started,
    but cpu1 was not started.

    zynq > /mnt/rwmem.elf 0xffff8000
    0x00000000ffff8000 = 0x00000000
    zynq > /mnt/rwmem.elf 0xfffffff0 0x18000000
    zynq > /mnt/rwmem.elf 0xffff8000
    0x00000000ffff8000 = 0x00000000
    zynq > /mnt/rwmem.elf 0xffff8000
    0x00000000ffff8000 = 0x00000000
    zynq > /mnt/rwmem.elf 0xffff8000
    0x00000000ffff8000 = 0x00000000

    "0xffff8000"address remains unchanged "0x00000000".

    Please provide a solution as soon as possible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    See answer on your duplicate post:

     

    http://zedboard.org/content/amp-running-linux-and-bare-metal-system-both-zynq-soc-processors-adapted-zedboard

     

    -Gary