Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development FreeRTOS & standalone version
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 737 views
  • Users 0 members are here
Related

FreeRTOS & standalone version

e14 Contributor
e14 Contributor over 14 years ago

In the FreeRTOS pdf it states:


  "This FreeRTOS port is not supported by Xilinx Technical Support and verification of this port is limited. This port is tested with v3_05a version of standalone BSP and will get updated for later releases. If the user needs to use later versions of standalone BSP released in 14.2 or later, he has to modify the version defined for the parameter standalone_version in the file <Xilinx_Zynq>/sw/repo/freertos_zynq_v1_00_a/data/freertos_zynq_v2_1_0.tcl."


  However this does not seem to work.  If the parameter is left at v3_05a, Everything compiles just fine,  but it is compiled against v3_05a, while the standalone version in the SDK is v3_06a.


  If the parameter in the file above is changed to v3_06, the tcl script seems to copy version 3_05a folder, but tries to compile against the v3_06va folder, which doesn't exist so it errors out. (while executing File ->New ->Xilinx Board Support Package)


  I can't figure out why v3_05a libraries are copied instead of v3_06a libraries, which is the root of the problem.


  Any help would be appretiated.

Ron

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 14 years ago

    Hi flostog,

    I have not gotten the 14.1 port to work but I did some searching around and I was able to locate this post on the FreeRTOS forums:

    http://interactive.freertos.org/entries/21922816-updated-xilinx-freertos-port-for-zynq-to-sdk-14-2-release

    I was able to download the attached archive from the above post and loosely follow the instructions from the PDF and get the example applications to run on ZedBoard.  I see the console output from the Hello World and see the LED blink from both of the LED applications.

    Of course, since the FreeRTOS port archive is targeted to ZC702, I had to use a very basic ZedBoard hardware platform where the instructions call out the basic ZC702 hardware platform.

    Also, for each of the LED applications, I changed the following definition to match ZedBoard LED hardware at LD9 on MIO7:

    #define OUTPUT_PINtt10t/* Pin connected to LED/Output */

    Changed to:

    #define OUTPUT_PINtt7t/* Pin connected to LED/Output */

    Everything seems to be working okay on my end so I suggest downloading the 14.2 tools and giving this a go.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 14 years ago

    Hi flostog,

    I have not gotten the 14.1 port to work but I did some searching around and I was able to locate this post on the FreeRTOS forums:

    http://interactive.freertos.org/entries/21922816-updated-xilinx-freertos-port-for-zynq-to-sdk-14-2-release

    I was able to download the attached archive from the above post and loosely follow the instructions from the PDF and get the example applications to run on ZedBoard.  I see the console output from the Hello World and see the LED blink from both of the LED applications.

    Of course, since the FreeRTOS port archive is targeted to ZC702, I had to use a very basic ZedBoard hardware platform where the instructions call out the basic ZC702 hardware platform.

    Also, for each of the LED applications, I changed the following definition to match ZedBoard LED hardware at LD9 on MIO7:

    #define OUTPUT_PINtt10t/* Pin connected to LED/Output */

    Changed to:

    #define OUTPUT_PINtt7t/* Pin connected to LED/Output */

    Everything seems to be working okay on my end so I suggest downloading the 14.2 tools and giving this a go.

    Regards,

    -Kevin