Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Booting kernel from sd card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 364 subscribers
  • Views 1552 views
  • Users 0 members are here
Related

Booting kernel from sd card

e14 Contributor
e14 Contributor over 10 years ago

Hi,

 

i 'am trying to build a sd card with Linaro from scratch. I have been to able to generate my boot.bin with first stage bootloader, bitstream and u-boot (from xilinx repository). I also have compiled my kernel (lastest version in xilinx repository) compiled the devi-tree file supplied with the kernel and setup my uEnv.txt with bootargs and bootcmd.

U-boot can load the kernel and boot it, but as soon as the kernel tries to mount a filessystem from sd card it crashed with the following message :

 

VFS: Cannot open root device "(null)" or unknown-block(0,0): error -6
Please append a correct "root=" boot option; here are the available partitions:
0100           16384 ram0  (driver?)
0101           16384 ram1  (driver?)
mmcblk0: mmc0:aaaa SL08G 7.40 GiB
 mmcblk0: p1 p2
0102           16384 ram2  (driver?)
0103           16384 ram3  (driver?)
0104           16384 ram4  (driver?)
0105           16384 ram5  (driver?)
0106           16384 ram6  (driver?)
0107           16384 ram7  (driver?)
0108           16384 ram8  (driver?)
0109           16384 ram9  (driver?)
010a           16384 ram10  (driver?)
010b           16384 ram11  (driver?)
010c           16384 ram12  (driver?)
010d           16384 ram13  (driver?)
010e           16384 ram14  (driver?)
010f           16384 ram15  (driver?)
1f00            1024 mtdblock0  (driver?)
1f01            5120 mtdblock1  (driver?)
1f02             128 mtdblock2  (driver?)
1f03            6016 mtdblock3  (driver?)
1f04            4096 mtdblock4  (driver?)
b300         7761920 mmcblk0  driver: mmcblk
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)

 

 

I first suspected that the default device tree config for zedboard does not have a correct clock configuration for the sdhc peripheral. But adding clokc frequency to the dts file did not work. Any idea of what i'am doing wrong ?

Thanks

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    I made some progress by doing the following :

    - choosing the right kernel for my vivado distribution

    - configuring bootargs straight into the kernel (at compile time)

    - using root=b302 instead of using root=/dev/mmcblk0p2

     

    since then the error changed a bit but still no boot for now :

    VFS: Cannot open root device "b302" or unknown-block(179,2): error -6

     

     

    any idea ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    I made some progress by doing the following :

    - choosing the right kernel for my vivado distribution

    - configuring bootargs straight into the kernel (at compile time)

    - using root=b302 instead of using root=/dev/mmcblk0p2

     

    since then the error changed a bit but still no boot for now :

    VFS: Cannot open root device "b302" or unknown-block(179,2): error -6

     

     

    any idea ?