Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development GPIO access on zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 364 subscribers
  • Views 842 views
  • Users 0 members are here
Related

GPIO access on zedboard

cascade99
cascade99 over 10 years ago

Hi
According to the following post, GPIO61 is the pin connect to LD6 on Zedboard, but when I try do "echo 61 < /sys/class/gpio/export", but I got error say "sh: write error: No such device", anybody knows which GPIO pin connecting a LED?
Thanks

http://zedboard.org/content/accessing-leds-and-switches-xillinux

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Lynn,

     

    You do not link to the post you reference, so it is difficult to know what your ZedBoard design should be doing.

     

    LD6 is connected to IO_0 of Bank 33 (pin U19) which is part of the PL (Programmable Logic) section of the Zynq device. It will not be connected to any GPIO until there is a bitstream loaded into the device and then it will depend on the design that generated the bitstream.

     

    You also do not mention what version of Linux you are using. There are differing offsets to the GPIO IO depending on the flavor and version of Linux.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cascade99
    0 cascade99 over 10 years ago in reply to e14 Contributor

    Thanks, Gary. I just put the link on the first post. Since I don't have any .bit file available yet. Do you know is there GPIO pin which can be controlled by MCU directly? I can access GPIO138/137, but couldn't verify I read/write them correctly.(they are floating I guess).
    I'm using petalinux 2014.4

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • cascade99
    0 cascade99 over 10 years ago in reply to e14 Contributor

    Thanks, Gary. I just put the link on the first post. Since I don't have any .bit file available yet. Do you know is there GPIO pin which can be controlled by MCU directly? I can access GPIO138/137, but couldn't verify I read/write them correctly.(they are floating I guess).
    I'm using petalinux 2014.4