Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development change default ipaddr of MicroZed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 364 subscribers
  • Views 490 views
  • Users 0 members are here
Related

change default ipaddr of MicroZed

e14 Contributor
e14 Contributor over 12 years ago

The default IP address of MicroZed is 192.168.1.10, I know this could be changed by typing command: ifconfig eth0 ***.***.***.***. but I don't want this kind of configuration work every time i start my board!
I'm wondering is there any method to set my board a certain ip, say for example, 192.168.1.9? To make sure it won't go back to the 192.168.1.10 every time i restart it.
At first, I thought the ipaddr is set by U-boot.elf, so I rebuild it with modification in directory "/include/configs/zynq_common.h" where there is a Macro defination "CONFIG_IPADDR", however the change I made here is not helpful, after I loaded u-boot.elf into my board's SD card, and let my os ran again, the ifconfig still showed me "192.168.1.10"
What should I do? .>_<.

  • Sign in to reply
  • Cancel
Parents
  • robertbrowder
    0 robertbrowder over 12 years ago

    Kay

    I am new to the microzed as well and needed the default netmask to be 255.255.0.0.  

    My somewhat hacked-up solution was to create a file /mnt/init.sh.   This is the last thing executed in the boot up process.   This file has only one line:

    "ifconfig eth0 192.168.1.10 netmask 255.255.0.0"

    There is probably a better way but this seemed to work for me.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • robertbrowder
    0 robertbrowder over 12 years ago

    Kay

    I am new to the microzed as well and needed the default netmask to be 255.255.0.0.  

    My somewhat hacked-up solution was to create a file /mnt/init.sh.   This is the last thing executed in the boot up process.   This file has only one line:

    "ifconfig eth0 192.168.1.10 netmask 255.255.0.0"

    There is probably a better way but this seemed to work for me.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to robertbrowder

    Robertbrowder
    Thank you, that works, init.sh is the file provided for customized initialization I guess. Just as what you put, this is the last thing executed in the boot up process, triggered by the last line "source /mnt/init.sh" in rcS file. I made changes by adding "ifconfig eth0 ***" in /etc/init.d/rcS, also works.
    Best regards