Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Error when using Zynq Demo Software
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 344 views
  • Users 0 members are here
Related

Error when using Zynq Demo Software

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I have been through a number of the demo application and they have run fine. I have moved on to using a demo that has a timer added to the Button/Led program and I now seem to be getting a constant crash when executing.

If I run the program in debug from the SDK it halts when Setting the direction of the LED GPIO. The specific error is Remote Failure reply: E01.

It happens at Xil_Out32. I am unsure whether the error above is because the system crashed or is the actual error itself in this function.

I hav rebuilt the entire solution from scratch, same problem. I have even rolled back by Vivado install to 2015.1 to check it wasn't the recent upgrade.

Anyone had the same issues?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hello James,

     

    Could you give us a little more information to go on. What board are you using? Can you provide a link to the demo software you are attempting to use? What version of Vivado does the demo software target? What is your host PC OS.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi Gary,


    Thanks for the reply;

    I am using the Zedboard and was using a demo from the "Zynq Book Tutorials", which is basically just a timer which counts up the LED's. (Windows OS)

    I appear to have resolved the issue by checking the Post Config ps7 option in the run configurations menu. I had read somewhere else that this sorts out the PS level shifters which was causing the issue when running in debug mode on the board.

    Thanks
    James