Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Digilent kernel in Xillinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 16 replies
  • Subscribers 364 subscribers
  • Views 1595 views
  • Users 0 members are here
Related

Digilent kernel in Xillinux

e14 Contributor
e14 Contributor over 14 years ago

I'm not sure if anybody else is having this problem, but I cannot get the full Digilent kernel to work for me with Xillinux.  Could anyone give an extremely dumbed-down step-by-step on how to do this?  I would appreciate it greatly.  Thanks.

  • Sign in to reply
  • Cancel
Parents
  • joswa
    0 joswa over 13 years ago

    I've used your .config to recompile the kernel and successfully build zImage file. I've replaced it with the zImage of a proven rich-kernel SD card (which can successfully run startx and go into ubuntu). However, the shell prompt redirected to serial port and the VGA monitor only displays the Xillybus image indefinitely. When I type "startx" in the serial port shell prompt, it reports "no screen is found".

    What went wrong? The behaviour is different from the pre-build rich-kernel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to joswa

    I will need some more details about what you did exactly: What kernel sources, which device tree, in short, exactly how your setting differs from the out-of-box Xillinux one (and which Xillinux version you differ from).

    I can only speculate that you've used your own kernel sources without patching them, so the driver for the VGA interface was not there. So as far as the kernel is concerned, there was no VGA adapter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to joswa

    I will need some more details about what you did exactly: What kernel sources, which device tree, in short, exactly how your setting differs from the out-of-box Xillinux one (and which Xillinux version you differ from).

    I can only speculate that you've used your own kernel sources without patching them, so the driver for the VGA interface was not there. So as far as the kernel is concerned, there was no VGA adapter.