Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Getting I2C up and running
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 366 subscribers
  • Views 2173 views
  • Users 0 members are here
Related

Getting I2C up and running

troy.cowan.123
troy.cowan.123 over 9 years ago

Hi. 

I'm trying to get the I2C functionality going in my application (running on a picozed).

As far as I can tell I've set up the PL correctly, enabling I2C 0 and connecting it to pins 50 and 51. In the PS, I'm using the iicps_v3_3 driver built into libxil.a. I'm calling the methods pretty much exactly as is done in the supplied example. When I attempt to send a couple of bytes out on the bus, nothing happens. I'm scoping the SCL and SDA lines, and they are not changing state at all. I never see the COMP bit or any error bit become active in the I2C registers. It's as though the I2C functionality is just inert or disabled. I'm stumped as far as how to troubleshoot this issue. Any help would be great, thanks!

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 9 years ago

    Hi Troy,

    Just making sure that I understand this correctly, you have configured your Vivado hardware platform to route one if the PS I2C controllers to MIO pins 50 and 51 and so you are not using the PL for any portion of the I2C interface, correct?

    Can you describe what you see on the SDA and SCL lines?  You mentioned that there is no toggling, are the lines stuck logic high or low?

    Best Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 9 years ago

    Hi Troy,

    Just making sure that I understand this correctly, you have configured your Vivado hardware platform to route one if the PS I2C controllers to MIO pins 50 and 51 and so you are not using the PL for any portion of the I2C interface, correct?

    Can you describe what you see on the SDA and SCL lines?  You mentioned that there is no toggling, are the lines stuck logic high or low?

    Best Regards,

    -Kevin