Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development debug build of BSP
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 471 views
  • Users 0 members are here
Related

debug build of BSP

e14 Contributor
e14 Contributor over 12 years ago

While trying to diagnose a problem I have been stepping into some BSP functions and it appears that the build is optimised. I get the usual weirdness single stepping the debugger through optimised code...

So, it turns out to be a bit complicated to make a debug build of the BSP - if I make the compiler setting '-g3' in BSP prefs the BSP link fails.

Is there an easy way to switch back and forth for the BSP?
(eg between '-g0' and '-g3' for gcc?)

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 12 years ago

    Hi Happy Heyoka,

    This question appears to be related to the Xilinx tools rather than MicroZed or ZedBoard specifically.  Please direct these types of tools questions to the Xilinx forums where you are more likely to get a response from the Xilinx experts.

    You should be able to override the optimization settings by appending an optimization flag (-O0 --> which is read hyphen, capital Oh, zero) to the extra_compiler_flags field.  This works okay for me to build the BSP in SDK.  Take a look at this forums post for further information:

    http://forums.xilinx.com/t5/Embedded-Development-Tools/How-to-turn-optimization-off-in-BSP/td-p/394275

    As for switching between a release BSP and a debug BSP, one thing that I do is to create two identical BSPs but set one to build with no optimization.  You can then change the referenced BSP for your application by right-clicking on the SDK project and selecting "Change Referenced BSP" menu option.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 12 years ago

    Hi Happy Heyoka,

    This question appears to be related to the Xilinx tools rather than MicroZed or ZedBoard specifically.  Please direct these types of tools questions to the Xilinx forums where you are more likely to get a response from the Xilinx experts.

    You should be able to override the optimization settings by appending an optimization flag (-O0 --> which is read hyphen, capital Oh, zero) to the extra_compiler_flags field.  This works okay for me to build the BSP in SDK.  Take a look at this forums post for further information:

    http://forums.xilinx.com/t5/Embedded-Development-Tools/How-to-turn-optimization-off-in-BSP/td-p/394275

    As for switching between a release BSP and a debug BSP, one thing that I do is to create two identical BSPs but set one to build with no optimization.  You can then change the referenced BSP for your application by right-clicking on the SDK project and selecting "Change Referenced BSP" menu option.

    Regards,

    -Kevin