Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development problem with programming the fpga on the zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 363 subscribers
  • Views 1702 views
  • Users 0 members are here
Related

problem with programming the fpga on the zedboard

e14 Contributor
e14 Contributor over 11 years ago

Hi,
I am having problem with my rev D zedboard. i am trying to program the fpga via the jtag port j17 using the supplied usb cable (only one usb cable is supplied which is also used for the uart connection). i have set all the   jumper (j7 to j11) correctly to ground. i am going through a zedbook tutorial and have reached the point in sdk to program the fpga via 'xilinx tools' -> program fpga but when i run this i get an error "program FPGA failed". what is wrong?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    You did not mention which Xilinx tools version you are using. I don't have a Windows XP machine to try, but using Windows 7 and Vivado SDK 2015.2, I was able to verify the xmd connection using one of the predefined hardware platforms. Also using Windows 7 I do hear a notification and see the USB serial converter connection in the Device Manager but do not get a 'hardware detected message'.

     

    Using a predefined zedboard hardware platform should rule out any errors you may have made in generating your design.

     

    First start up SDK (no need for a Vivado design for this exercise). Setup a workspace directory for your experiment.

     

    Once SDK is started 'Create Application'.

     

    Then, under 'FIle' on the SDK toolbar select 'New" > 'Application Project'.

     

    Give the project a name and them select 'zed_hw_platform' in the 'Hardware Platform' selection. Make sure 'Create New' is selected for the Board Support Package and then click 'Next'.

     

    Select 'Hello World' and then 'Finish'.

     

    Once the application has been generated select 'XMD Console' under 'Xilinx Tools' on the SDK toolbar.

     

    In the XDM console that opens type "connect arm hw".

     

    If XDM is able to connect to the Zedboard successfully that should verify your hardware.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Thanks Gary. I used the connect arm hw command in XDM and it worked.
    Many thanks for your help.

    mehrdad

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Thanks Gary. I used the connect arm hw command in XDM and it worked.
    Many thanks for your help.

    mehrdad