Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development problem with programming the fpga on the zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 363 subscribers
  • Views 1702 views
  • Users 0 members are here
Related

problem with programming the fpga on the zedboard

e14 Contributor
e14 Contributor over 11 years ago

Hi,
I am having problem with my rev D zedboard. i am trying to program the fpga via the jtag port j17 using the supplied usb cable (only one usb cable is supplied which is also used for the uart connection). i have set all the   jumper (j7 to j11) correctly to ground. i am going through a zedbook tutorial and have reached the point in sdk to program the fpga via 'xilinx tools' -> program fpga but when i run this i get an error "program FPGA failed". what is wrong?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    I am having problem with my rev D zedboard. I have windows 10 and the version of the Xilinx tools that I use are Vivado 2015.4. i am trying to program the fpga via the jtag port j17 using the supplied usb cable (only one usb cable is supplied which is also used for the uart connection). i have set all the jumper (j7 to j11) correctly to ground.   i am going through a zedbook tutorial and have reached the point in sdk to program the fpga via 'xilinx tools' -> program fpga but when i run this i get an error "program FPGA failed".  the error massage said : " could not find the FPGA defice on the board for connection 'local'."
    the troubleshooting hints:
    check wheher board is connecting to the system properly.
    check the switch power.
    I checked every thing but it does not work.
    when I opened Windows Device Manager, and I see the "USB Serial Converter" added to the hardware list.
    So, what is wrong?
    can you help me with clear steps to fix it.
    Also, If you have video or picture, please send it to my email :
    jhs.jhs2007@hotmail.com

    thank you
    Saleh
    ^_^
     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    I am having problem with my rev D zedboard. I have windows 10 and the version of the Xilinx tools that I use are Vivado 2015.4. i am trying to program the fpga via the jtag port j17 using the supplied usb cable (only one usb cable is supplied which is also used for the uart connection). i have set all the jumper (j7 to j11) correctly to ground.   i am going through a zedbook tutorial and have reached the point in sdk to program the fpga via 'xilinx tools' -> program fpga but when i run this i get an error "program FPGA failed".  the error massage said : " could not find the FPGA defice on the board for connection 'local'."
    the troubleshooting hints:
    check wheher board is connecting to the system properly.
    check the switch power.
    I checked every thing but it does not work.
    when I opened Windows Device Manager, and I see the "USB Serial Converter" added to the hardware list.
    So, what is wrong?
    can you help me with clear steps to fix it.
    Also, If you have video or picture, please send it to my email :
    jhs.jhs2007@hotmail.com

    thank you
    Saleh
    ^_^