Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development problem with programming the fpga on the zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 363 subscribers
  • Views 1700 views
  • Users 0 members are here
Related

problem with programming the fpga on the zedboard

e14 Contributor
e14 Contributor over 11 years ago

Hi,
I am having problem with my rev D zedboard. i am trying to program the fpga via the jtag port j17 using the supplied usb cable (only one usb cable is supplied which is also used for the uart connection). i have set all the   jumper (j7 to j11) correctly to ground. i am going through a zedbook tutorial and have reached the point in sdk to program the fpga via 'xilinx tools' -> program fpga but when i run this i get an error "program FPGA failed". what is wrong?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Saleh,

     

    Windows 10 is not a supported host OS for Vivado at this point. Based on these posts on the Xilinx Community forums it looks like others have run into your cable/programming issue with Windows 10.

     

    https://forums.xilinx.com/t5/Installation-and-Licensing/Windows-10/td-p/645652/highlight/true/page/3

     

    https://forums.xilinx.com/t5/Design-Tools-Others/vivado-2015-3-on-Windows10/td-p/663466

     

    You might try posting on the Xilinx Community forums development tools forum to see if anyone has managed to make it work. There are also posts on the Xilinx forums that indicate that there are plans to support Windows 10 in Vivado 2016.x, but they are not specific as to which 2016 release it will be.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Saleh,

     

    Windows 10 is not a supported host OS for Vivado at this point. Based on these posts on the Xilinx Community forums it looks like others have run into your cable/programming issue with Windows 10.

     

    https://forums.xilinx.com/t5/Installation-and-Licensing/Windows-10/td-p/645652/highlight/true/page/3

     

    https://forums.xilinx.com/t5/Design-Tools-Others/vivado-2015-3-on-Windows10/td-p/663466

     

    You might try posting on the Xilinx Community forums development tools forum to see if anyone has managed to make it work. There are also posts on the Xilinx forums that indicate that there are plans to support Windows 10 in Vivado 2016.x, but they are not specific as to which 2016 release it will be.

     

    -Gary