Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Kernel Upgrade, broken SPI
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 1302 views
  • Users 0 members are here
Related

Kernel Upgrade, broken SPI

buckd
buckd over 10 years ago

Hi,

I am using a MicroZed 7z010 with Linux kernel 3.9.0 (xilinx-v14.6.02) from:

https://github.com/Xilinx/linux-xlnx/

I am attempting to upgrade the kernel to the latest version (4.4.0) from the same repo but it broke the SPI communication to an Analog Devices PLL that is connected.  The spidev module in the kernel is enabled, as well as all the other xilinx/zynq modules.  A C program is run, using spidev, to communicate to the PLL.

The two main issues I am seeing are:

  1.   SPI transfer timed out after every byte (either transfering the bytes one-by-one or using the C function 'SPI_IOC_MESSAGE'.
  2.   With an oscilloscope, I see that the chip-select signal starts high when rebooting the board, but then stays low after the first transfer attempt - the old kernel would return it to high.


I admit that I'm a bit new to using this technology, but I have Linux and C experience.  Things that I have attempted:

  •   Modifying the device-tree in dozens of ways
  •   Modified the SPI C code to send SPI using a number of different parameters
  •   Modified the Linux kernel module (spi.c and/or spi-cadence.c)
  •   Too much trial-and-error


The best of the outcomes would still give me those two problems mentioned above.

Is there something I'm doing wrong?

Thanks for any help!

  • Sign in to reply
  • Cancel
Parents
  • buckd
    0 buckd over 10 years ago

    Here are my device tree settings (because otherwise the first post would have been marked as SPAM):

    The old device tree looks like this (kernel 3.9.0):

            ps7-spi@e0007000 {
                #addresss-cells = <0x1>;
                #size-cells = <0x0>;
                bus-num = <0x0>;
                compatible = "xlnx,ps7-spi-1.00.a";
                interrupt-parent = <0x1>;
                interrupts = <0x0 0x31 0x4>;
                num-chip-select = <0x4>;
                reg = <0xe0007000 0x1000>;
                speed-hz = <0xf42400>;
                xlnx,has-ss0 = <0x0>;
                xlnx,has-ss1 = <0x1>;
                xlnx,has-ss2 = <0x0>;
                xlnx,spi-clk-freq-hz = <0xf42400>;

                device@0 {
                    compatible = "rohm,dh2228fv";
                    spi-max-frequency = <0x3d0900>;
                    reg = <0x0>;
                };
            };

    The new looks like this (kernel 4.4.0, I know this is very messy):

            spi@e0007000 {
                compatible = "xlnx,zynq-spi-r1p6";
                reg = <0xe0007000 0x1000>;
                interrupt-parent = <0x3>;
                interrupts = <0x0 0x31 0x4>;
                clocks = <0x1 0x1a 0x1 0x23>;
                clock-names = "ref_clk", "pclk";
                #address-cells = <0x1>;
                #size-cells = <0x0>;
                num-chip-select = <0x4>;
                num-cs = <0x4>;
                speed-hz = <0xf42400>;
                xlnx,has-ss0 = <0x0>;
                xlnx,has-ss1 = <0x1>;
                xlnx,has-ss2 = <0x0>;
                xlnx,spi-clk-freq-hz = <0xf42400>;
                
                device@0 {
                    compatible = "rohm,dh2228fv";
                    spi-max-frequency = <0x3d0900>;
                    reg = <0x0>;
                };
            };

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • buckd
    0 buckd over 10 years ago

    Here are my device tree settings (because otherwise the first post would have been marked as SPAM):

    The old device tree looks like this (kernel 3.9.0):

            ps7-spi@e0007000 {
                #addresss-cells = <0x1>;
                #size-cells = <0x0>;
                bus-num = <0x0>;
                compatible = "xlnx,ps7-spi-1.00.a";
                interrupt-parent = <0x1>;
                interrupts = <0x0 0x31 0x4>;
                num-chip-select = <0x4>;
                reg = <0xe0007000 0x1000>;
                speed-hz = <0xf42400>;
                xlnx,has-ss0 = <0x0>;
                xlnx,has-ss1 = <0x1>;
                xlnx,has-ss2 = <0x0>;
                xlnx,spi-clk-freq-hz = <0xf42400>;

                device@0 {
                    compatible = "rohm,dh2228fv";
                    spi-max-frequency = <0x3d0900>;
                    reg = <0x0>;
                };
            };

    The new looks like this (kernel 4.4.0, I know this is very messy):

            spi@e0007000 {
                compatible = "xlnx,zynq-spi-r1p6";
                reg = <0xe0007000 0x1000>;
                interrupt-parent = <0x3>;
                interrupts = <0x0 0x31 0x4>;
                clocks = <0x1 0x1a 0x1 0x23>;
                clock-names = "ref_clk", "pclk";
                #address-cells = <0x1>;
                #size-cells = <0x0>;
                num-chip-select = <0x4>;
                num-cs = <0x4>;
                speed-hz = <0xf42400>;
                xlnx,has-ss0 = <0x0>;
                xlnx,has-ss1 = <0x1>;
                xlnx,has-ss2 = <0x0>;
                xlnx,spi-clk-freq-hz = <0xf42400>;
                
                device@0 {
                    compatible = "rohm,dh2228fv";
                    spi-max-frequency = <0x3d0900>;
                    reg = <0x0>;
                };
            };