Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Kernel Upgrade, broken SPI
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 1300 views
  • Users 0 members are here
Related

Kernel Upgrade, broken SPI

buckd
buckd over 10 years ago

Hi,

I am using a MicroZed 7z010 with Linux kernel 3.9.0 (xilinx-v14.6.02) from:

https://github.com/Xilinx/linux-xlnx/

I am attempting to upgrade the kernel to the latest version (4.4.0) from the same repo but it broke the SPI communication to an Analog Devices PLL that is connected.  The spidev module in the kernel is enabled, as well as all the other xilinx/zynq modules.  A C program is run, using spidev, to communicate to the PLL.

The two main issues I am seeing are:

  1.   SPI transfer timed out after every byte (either transfering the bytes one-by-one or using the C function 'SPI_IOC_MESSAGE'.
  2.   With an oscilloscope, I see that the chip-select signal starts high when rebooting the board, but then stays low after the first transfer attempt - the old kernel would return it to high.


I admit that I'm a bit new to using this technology, but I have Linux and C experience.  Things that I have attempted:

  •   Modifying the device-tree in dozens of ways
  •   Modified the SPI C code to send SPI using a number of different parameters
  •   Modified the Linux kernel module (spi.c and/or spi-cadence.c)
  •   Too much trial-and-error


The best of the outcomes would still give me those two problems mentioned above.

Is there something I'm doing wrong?

Thanks for any help!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hey,

    I am sorry but this is not a solution to your problem but rather I hope to seek some advice from you. Since you say that your SPI interface broke with the new Kernel, I assume it was working earlier. 

    I am trying to interface an accelerometer, ADXL345 using SPI with the zedboard, with petalinux installed on it. However I am unable to do so. I do not want to sidetrack the discussion from your issue so I will not post further about my problem here however I will be extremely grateful if you could take a look at my problem at this link.

    http://zedboard.org/content/trying-interface-adxl345-using-spi

    If you do not know a possible solution can you please tell the changes you made to your device tree to enable the driver etc.

    Thanks

    Shubham Sharma

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hey,

    I am sorry but this is not a solution to your problem but rather I hope to seek some advice from you. Since you say that your SPI interface broke with the new Kernel, I assume it was working earlier. 

    I am trying to interface an accelerometer, ADXL345 using SPI with the zedboard, with petalinux installed on it. However I am unable to do so. I do not want to sidetrack the discussion from your issue so I will not post further about my problem here however I will be extremely grateful if you could take a look at my problem at this link.

    http://zedboard.org/content/trying-interface-adxl345-using-spi

    If you do not know a possible solution can you please tell the changes you made to your device tree to enable the driver etc.

    Thanks

    Shubham Sharma