Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development BSP and Xilinx SDK
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 801 views
  • Users 0 members are here
Related

BSP and Xilinx SDK

ist_ali
ist_ali over 9 years ago

Hello:

Just bought MicroZed Industry4.0 Ethernet kit and tried to use Xilinx SDK to create hello world project. Which BSP should I use? Also tried to run memory test but it failed. Any idea about this?

Thanks,

Andrew

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Andrew,

    You will want to use one of the MicroZed 7020 BSPs located at :

    http://zedboard.org/support/design/1519/10

    I would personally suggest the newest BSP "PetaLinux 2016.2 Compressed BSP, z7020"

    As for your board not passing the run memory test. I am under the impression that somthing in your hardware design is setup incorrectly. I am going to suggest you run through labs 01-03 to make sure everything works correctly. You can find them at:

    http://zedboard.org/support/design/1519/10

    In these labs you will only use your MicroZed SOM (No carrier card)

    Here is what you will do in these labs

     

    Tutorial 01 Build the Zynq Hardware Platform - Here you will construct your hardware design

    Tutorial 02 First Application Hello World - Here you will import the hardware design to SDK and then create and run the Hello World application

    Tutorial 03 Test Applications - Here you will create the Test Peripheral and Test Memory applications and run them

    *** One thing of note is to make sure you download the lab material that corresponds to your currently installed Vivado Version. 

    Plese report back if Tutorial 03 is a success or failure

    Thanks,

    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ist_ali
    0 ist_ali over 9 years ago in reply to jafoste4

    Hi Josh:

    Thanks for the info. 

    When I followed the steps to create Zynq hardware platform in Vivado, there's only one board, Zedboard Zynq evaluation..., shown in the panel. There's no MicroZed or PicoZed boards listed. 

    Thanks,

    Andrew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ist_ali
    0 ist_ali over 9 years ago in reply to jafoste4

    Hi Josh:

    Thanks for the info. 

    When I followed the steps to create Zynq hardware platform in Vivado, there's only one board, Zedboard Zynq evaluation..., shown in the panel. There's no MicroZed or PicoZed boards listed. 

    Thanks,

    Andrew