Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development I want to use UART0 and UART1, but no output
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 761 views
  • Users 0 members are here
Related

I want to use UART0 and UART1, but no output

e14 Contributor
e14 Contributor over 10 years ago

Hi all,
I can run the linux kernel  on my custom zedboard, where the output message is come from UART1.However, I hope to use UART1 and UART0 at the same time. I have set the pin of MIO 10 and MIO 11 for uart0 in vivado2015 configuration and enabled the UART0 port.

I also added the uart0 infomation on my diglient_zynq.dts.

aliases{

etherner0=&ps_etherner_0;

serial1=&ps7_uart_0;

serial0=&ps7_uart_1;

} 

...

pa7_uart_0:serial@e0000000{

clock=<50000000>

clock-frequency=<50000000>

device_type="serial"

interrupts=<0,27,4>

....

}

pa7_uart_1:serial@e0001000{

clock=<50000000>

clock-frequency=<50000000>

device_type="serial"

interrupts=<0,50,4>

....

}

In my opnion, the UART0 has been defined correctly in that file.

Generaly, kernel will print:
----------------------------
e0001000.uart: ttyPS0 at MMIO 0xe0001000 (irq = 82) is a xuartps
console [ttyPS0] enabled
e0000000.uart: ttyPS1 at MMIO 0xe0000000 (irq = 59) is a xuartps
----------------------------
Unfortunately, I can't find any message about "ttyPS1" from kernel output.
Has any one can help me or give me any tips??

ps:i using the cmd "cat proc/interupts",i find the irq 82,but i can't find the irq 59,i have no reason why did this problem.

Thanks!

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 10 years ago

    Hello Zhudouhuifei,

    I have found some reference posts where they are trying to implement both Uarts for their Zynq device. Try looking, and comparing them to solve your issue.

    http://zedboard.org/content/enabling-uart-0

    http://zedboard.org/content/uart-application

    http://zedboard.org/content/uart-0-hangs-when-uart-1-receive-data-amp

    https://forums.xilinx.com/t5/Embedded-Linux/Enabling-the-second-UART-on-the-ZC702-Zynq-Dev-Board/td-p/236674

    https://forums.xilinx.com/t5/Zynq-All-Programmable-SoC/Problem-using-two-uarts-with-a-Zynq-First-Stage-Boot-Loader-BSP/td-p/550946

    --Josh