Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Zynq Concepts, Tools, and Techniques on ZedBoard - Issues
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 364 subscribers
  • Views 1959 views
  • Users 0 members are here
Related

Zynq Concepts, Tools, and Techniques on ZedBoard - Issues

e14 Contributor
e14 Contributor over 13 years ago


Hi all,

I'm new to the Zedboard, running through the 14.3 CTT tutorial, and I've encountered two problems:

1) Section 3.1.2 - The application code does not compile without error:

../src/helloworld.c:39:6: error: conflicting types for 'print'
../../Hello_world_bsp/ps7_cortexa9_0/include/xil_printf.h:39:6: note: previous declaration of 'print' was here
make: *** [src/helloworld.o] Error 1

To compile, the following line must be removed/commented:
void print(char *str);


2) The expanded Helloworld.c example contained in Appendix A crashes when run on hardware (within the SDK). After an open is selected (pressing '1' for example), a popup Terminal Error message appears :"IO Error! Bad file descriptor in nativeDrain"

##### Application Starts #####

SELECT the Operation from the Below Menu
###################### Menu Starts ########################
Press '1' to use NORMAL GPIO as an input (BTNU switch)
Press '2' to use EMIO as an input (BTNR switch)
Press any other key to Exit
##################### Menu Ends #########################
Selection : 1
Press Switch 'BTNU' push button on
Bad file descriptor in nativeDrain
board

I haven't found a resolution yet to the nativeDrain error. Has anyone encountered similar issues? I've tried this on two PC's (Win7), same result.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I have the same issue,
    When running the program, the output from zedboard is displayed on putty terminal properly(i.e. all the print commands works fine) but on pressing '1' or '2' from keyboard I do not see any action on the terminal. To troubleshoot, I hard-coded the value '1'  and the program worked fine then. Hence, there is some issue with the "inbyte()" command and program is stuck there. Can anybody please provide any help regarding that.
    I am using vivado 2013.3 and following the 2013.4 version of the document bcs i could not find any for 2013.3
    P.S. - already completed all the steps necessary related to cypress driver.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Is the 'Putty' terminal window selected when you are pressing the keys?

     

    If so you might want to try the Out of the Box Linux provided with the ZedBoard to verify that you are able to input in the Putty terminal with a known good application.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Is the 'Putty' terminal window selected when you are pressing the keys?

     

    If so you might want to try the Out of the Box Linux provided with the ZedBoard to verify that you are able to input in the Putty terminal with a known good application.

     

    -Gary