Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development compiling freeRTOS for microZed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 364 subscribers
  • Views 817 views
  • Users 0 members are here
Related

compiling freeRTOS for microZed

e14 Contributor
e14 Contributor over 11 years ago

I can't find any starting point for compiling freeRTOS for microzed.

I have been working on ZYNQ for more than a year, but first time trying to get FreeRTOS on microZed. Is there any starting point/tutorial/documentation for FreeRTOS on microZed?

Thanks
BlueHatSoft Dev.

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 11 years ago

    Hi bluehatsoft,

    I did some searching and have found that others are running FreeRTOS on ZedBoard so the steps to get that working should be very similar for MicroZed.

    http://forums.xilinx.com/t5/Embedded-Development-Tools/Where-is-Xilinx-FreeRTOS-for-Zynq-using-SDK-2014/td-p/535503

    Here are some additional resources that may be useful:

    http://www.wiki.xilinx.com/FreeRTOS

    http://www.freertos.org/RTOS-Xilinx-Zynq.html

    If you get this working, please share your results back with the community.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to zedhed

    The main Zynq project in the FreeRTOS download uses the Xilinx SDK and comprises three projects - the hardware definition, the BSP generated from the hardware definition, and the application - so the application is decoupled from the hardware.  To move the application to a different hardware platform then you 'just' need to get the SDK to generate a BSP for that hardware platform, then link the application to the new BSP.  You may need to change the IO ports for the new hardware - for example, which IO an LED is connected to etc.

    In addition to the link already posted, the following link shows you how to get the SDK itself to generate a simply blinky demo for the Zynq (although the full demo on the previously posted link provides a more comprehensive example):
    http://www.freertos.org/RTOS-Xilinx-SDK-BSP.html

    Further, in about a week (hopefully less) or so we will be releasing a full FreeRTOS+TCP (http://www.FreeRTOS.org/tcp) and FreeRTOS+FAT (http://www.FreeRTOS.org/fat) demo for the Zynq.  This has FTP and basic HTTP functionality, and has been developed by my colleague on a microZed board, and I have been testing it on a ZC702 - so it is shipping with both hardware definitions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 11 years ago

    Hi bluehatsoft,

    I almost forgot to mention that Adam Taylor had a few parts of the MicroZed Chronicles that showed how to get a simple FreeRTOS application up and running on MicroZed:

    http://forums.xilinx.com/t5/Xcell-Daily-Blog/Adam-Taylor-s-MicroZed-Chronicles-Part-44-MicroZed-Operating/ba-p/499282

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The FreeRTOS+TCP and FreeRTOS+FAT project for the Zynq has now been published.  It contains hardware designs for microZed as well as ZC702.

    http://www.freertos.org/FreeRTOS-Plus/FreeRTOS_Plus_TCP/TCPIP_FAT_Examples_Xilinx_Zynq.html

    Support is available on the link below.  The same link can be used to provide constructive feedback - which is always gratefully received.
    http://www.freertos.org/FreeRTOS_Support_Forum_Archive/freertos_support_forum_archive_index.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    I got the application working following the tutorial. thanks