Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development triple frame buffer
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 926 views
  • Users 0 members are here
Related

triple frame buffer

kcox@sgss.com
kcox@sgss.com over 9 years ago

Hello

I have an application that uses the VDMA core for transferring video from camera IP to  DDR on a Zynq 7020 (bare metal application).  I am using the default number of frame buffers (3).  My application uses interrupts to notify when a frame buffer transfer has completed.  I have setup the VDMA driver for circular buffer mode.  I read the buffers from DDR in the following order 0,1,2,0,1,2... (Normal circular buffer processing) when an interrupt fires.  When I look at the images, the first cycle through all the buffers looks good.  After the first cycle buffer 0 stays the same and only buffer 1 and 2 change.  I'm not sure if I understand now what triple buffering means in the VDMA context.  Is it not just a simple ring buffer that constantly cycles though the buffers in the order 0-1-2.

 

Kevin

  • Sign in to reply
  • Cancel
Parents
  • kcox@sgss.com
    0 kcox@sgss.com over 9 years ago

    I fixed the problem by disabling the read channel in the VDMA core.  I am working with a reference design that used both the read and write channels of the VDMA core.  I modified the design and removed the connections from the M_AXIS_MM2S port so that the DMA core was no longer outputting data to the HDMI logic.  But I did not check the box in the DMA core that disables the read channel.  This must cause confusion internal to the DMA core as I also had the GenLock logic activated that keeps the read and write channels in sync.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • kcox@sgss.com
    0 kcox@sgss.com over 9 years ago

    I fixed the problem by disabling the read channel in the VDMA core.  I am working with a reference design that used both the read and write channels of the VDMA core.  I modified the design and removed the connections from the M_AXIS_MM2S port so that the DMA core was no longer outputting data to the HDMI logic.  But I did not check the box in the DMA core that disables the read channel.  This must cause confusion internal to the DMA core as I also had the GenLock logic activated that keeps the read and write channels in sync.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer