Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Simple AxiDma on Microzed, unexpected behaviour
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 670 views
  • Users 0 members are here
Related

Simple AxiDma on Microzed, unexpected behaviour

dune_userfog
dune_userfog over 9 years ago

Hello,
I'm using a Microzed (7010) Evaluation Kit with Vivado (2016.3) and SDK (2016.3) on Win7 Pro/64bit.

I developed a simple standalone AxiDma application in order to transfer two blocks of data of size = 0xC0000 bytes (786432 bytes) toward the DDR.
Each transfer is performed by calling XAxiDma_SimpleTransfer(...,(STARTADDR+i*size), size, ....) and then waiting for transfer completation (XaxiDma_Busy(..)) before starting the next one.
 
It works fine with STARTADDR >= 0x00110000, however it fails or blocks if STARTADDR = 0x00100000 or smaller than 0x0010E000 (about).

All suggestions are welcome.
Thank you

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Dune,

    In our Developing Zynq Hardware Speedway, located in the supporting documents we have a proven AXI DMA application. I am going to suggest you download it and refer to it for your debug process.

    You can find it at : http://zedboard.org/course/developing-zynq%C2%AE-7000-all-programmable-soc-hardware-vivado-20133-201441-20152-and-20162

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dune_userfog
    0 dune_userfog over 9 years ago in reply to jafoste4

    Thanks for suggestion regarding code examples.
    I've seen the BRAM example and the offset used for DDR start address to pass code and data sections.

    Thank you very much for the useful support.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer