Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Xilinx Zynq Base TRD 14.3 on Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 364 subscribers
  • Views 560 views
  • Users 0 members are here
Related

Xilinx Zynq Base TRD 14.3 on Zedboard

shakith
shakith over 13 years ago

Hi all,

I got hardware and bare metal software of Zynq Base TRD 14.3 reference design working on the zedboard.  Starting from this (http://wiki.analog.com/resources/tools-software/linux-drivers/platforms/zynq#enable_xf86-video-modesetting_xorg_driver) working design I added the VDMA_filter and sobel_filter_engine and wrote a simple test program to send the image to the filter and to get back the filtered image and display both on the hdmi output.

Next step, I want to get linux drivers working on this kernel tree that supports zedboard.(e.g. https://github.com/Digilent/linux-3.3-digilent.)

This hardware design uses a vdma for the hdmi output (this is in addition to the vdma for the filter operations). I added the patch from (http://wiki.xilinx.com/zynq-base-trd-14-3). This patch adds two drivers: xvdma (for vdma filter) and xfilter (for filter engine). Xvdma is extended driver of the xilinx_dma driver. With few minor tweaks I managed to compile the kernel. At bootup, when the device tree file doesnu2019t contain the entries for new vdma_filter and filter_engine, the kernel crashes at a line from xvdma (static bool xvdma_filter(struct dma_chan *chan, void *param). This means, vdma_hdmi is also somehow also to trying to run the xvdma driver.

I added a compatibility string to the xvdma driver (the extended driver) such that device tree entry for the vdma_hdmi only matches xilinx_dma driver and it doesnu2019t match xvdma driver. But it still crashes at the above point.

Alternatively is it possible to get user space access to the hardware to run my bare metal application earlier? I guess the memory mapped register IO access should be alright, but DMA access might be an issue?
Thanks in advance.

Cheers
Shakith

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hello,everyone ! i am using the ISE 14.4,and i want to write some driver for linux 3.6.0,but i don't know how to build the kernel source tree, i have downloaded the kernel file,and i want your help,please !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hello,everyone ! i am using the ISE 14.4,and i want to write some driver for linux 3.6.0,but i don't know how to build the kernel source tree, i have downloaded the kernel file,and i want your help,please !