Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development MicroZed U-boot for Flash
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 600 views
  • Users 0 members are here
Related

MicroZed U-boot for Flash

e14 Contributor
e14 Contributor over 11 years ago

I am working with a MicroZed board and I have been trying to get u-boot to be able to access the flash using the sf probe command. I downloaded the MicroZed_Open_Source_Linux_In_System_QSPI_Programming_14_5_02-Tutorial from the MicroZed tutorial page and have been able to use the files provided without any issue. I have wanted to change a few configs in u-boot and generate my own u-boot file, but my u-boot cannot find the qspi flash, so I have no access to it. If I use the provided u-boot.elf from the download, I can access the flash with no problem, thus I know that the problem is u-boot and not my fsbl. I would just use the u-boot that is provided but then I wouldn't be able to change my configurations as I would like them to be. When I use the sf probe command in u-boot, I get an error saying:

Invalid bus 0 (err=-19)
Failed to initialize SPI flash at 0:0 (error -19)

Does anyone know how to resolve this issue or know where I can obtain the .config file for the u-boot that is provided in the tutorial so that I can replicate the configuration?

Thanks

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 11 years ago

    Hi Jordan,

     

    What version of U-boot are you using for your U-Boot and where does it come from?

     

    At the time U-boot was built using the source on the Xilinx Git repository from the xilinx-v14.5 release tag.

    https://github.com/Xilinx/u-boot-xlnx

     

    You could start with that and simply use the zed defconfig and it should give you the QSPI support you need.

     

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to zedhed

    Kevin,

    Thank you for responding so quickly, I am currently using the newest xilinx version of u-boot. I will try using xilinx-v14.5 and see if that works for me.

    Thanks,
    Jordan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to zedhed

    Kevin,

    It looks like that was exactly what I was looking for. I will be able to work with that now and configure it how I would like. Thanks for your help.

    Jordan