Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Petalinux SPI driver running but not connecting
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 367 subscribers
  • Views 3737 views
  • Users 0 members are here
Related

Petalinux SPI driver running but not connecting

cuevas1208
cuevas1208 over 9 years ago

I am having issues with my Petalinux SPI driver.

I have successfully tested on Xilinx SDK by using one of their spi templates and it worked just fine, but when I tried to set it up on Petalinux the programs runs but it can not connect.  It looks like Petalinux can not connect to the FPGA, what can I do to get it working?

This what I get after running the code:

root@pz-7020-2016-2:/bin# ./spidev_test -D /dev/spidev32766.0 --speed 10000000
spi mode: 0x0
bits per word: 8
max speed: 10000000 Hz (10000 KHz)
spidev spi32766.0: SPI transfer timed out
can't send spi message: Connection timed out
Aborted

I using PetalinuxTools16.2, and Vivado 16.2. 

Click here to see my dts files, and my spidev_test.c.

Block diagram:

 

Fullscreen contentimage_80103.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

Here are the steps I have done to set the SPI driver:

  1.  

    I created a project:

     
        
    1.    

      petalinux-create --type project --template zynq --name petalinux_pz_7020 --source pz_7020_2016_2.bsp

        
    2.  
  2.  

    I import my hardware:

     
        
    1.    

      petalinux-config --get-hw-description vivado_Project/vivado_pz_7020.sdk --project petalinux_pz_7020

        
    2.  
  3.  

    Created an app

     
        
    1.    

      petalinux-create -t apps --name spidev --template c

        
    2.  
  4.  

    I replace the content of the app spidev.c for the spidev_test.c attached to this email.

  5.  

    Enable SPI support for your kernel:

     
        
    1.    

      Navigate to Device Drivers->SPI support and make sure that Cadence SPI controller, Xilinx SPI controller command module, Xilinx Zynq QSPI controller, and User mode SPI device driver support are all enabled.

        
    2.  
  6.  

    Enabled the new app

     
        
    1.    

      $ petalinux-config -c rootfs  

        
    2.   
    3.    

      Apps->spidev (Press Y to select the application)

        
    4.  
  7.  

    Build petalinux image

     
        
    1.    

      petalinux-build

        
    2.  
  8.  

    Package the distribution

     
        
    1.    

      petalinux-package  --boot --fsbl images/linux/zynq_fsbl.elf --fpga ../vivado_Project/impl_1/blockDesign_wrapper.bit --uboot --kernel --force

        
    2.  
  9.  

    Update Firmware

     
        
    1.    

      run netboot  

        
    2.  

Note:

In my petalinux project under /dev ia can see spidev32766.0, and under /bin I can see spidev

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 9 years ago

    Hi cuevas1208,

    Can you please post the contents of your spidev.c Linux app here?

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cuevas1208
    0 cuevas1208 over 9 years ago in reply to zedhed

     
      
       
        
         
          
           
    
    /*
     * SPI testing utility (using spidev driver)
     *
     * Copyright (c) 2007  MontaVista Software, Inc.
     * Copyright (c) 2007  Anton Vorontsov <avorontsov@ru.mvista.com>
     *
     * This program is free software; you can redistribute it and/or modify
     * it under the terms of the GNU General Public License as published by
     * the Free Software Foundation; either version 2 of the License.
     *
     * Cross-compile with cross-gcc -I/path/to/cross-kernel/include
     */
    
    #include <stdint.h>
    #include <unistd.h>
    #include <stdio.h>
    #include <stdlib.h>
    #include <string.h>
    #include <getopt.h>
    #include <fcntl.h>
    #include <sys/ioctl.h>
    #include <linux/types.h>
    #include <linux/spi/spidev.h>
    
    #define ARRAY_SIZE(a) (sizeof(a) / sizeof((a)[0]))
    
    static void pabort(const char *s)
    {
     perror(s);
     abort();
    }
    
    static const char *device = "/dev/spidev32765.0";
    static uint32_t mode;
    static uint8_t bits = 8;
    static uint32_t speed = 500000;
    static uint16_t delay;
    static int verbose;
    
    uint8_t default_tx[] = {
     0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF,
     0x40, 0x00, 0x00, 0x00, 0x00, 0x95,
     0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF,
     0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF,
     0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF,
     0xF0, 0x0D,
    };
    
    uint8_t default_rx[ARRAY_SIZE(default_tx)] = {0, };
    char *input_tx;
    
    static void hex_dump(const void *src, size_t length, size_t line_size, char *prefix)
    {
     int i = 0;
     const unsigned char *address = src;
     const unsigned char *line = address;
     unsigned char c;
    
     printf("%s | ", prefix);
     while (length-- > 0) {
      printf("%02X ", *address++);
      if (!(++i % line_size) || (length == 0 && i % line_size)) {
       if (length == 0) {
        while (i++ % line_size)
         printf("__ ");
       }
       printf(" | ");  /* right close */
       while (line < address) {
        c = *line++;
        printf("%c", (c < 33 || c == 255) ? 0x2E : c);
       }
       printf("\n");
       if (length > 0)
        printf("%s | ", prefix);
      }
     }
    }
    
    /*
     *  Unescape - process hexadecimal escape character
     *      converts shell input "\x23" -> 0x23
     */
    static int unescape(char *_dst, char *_src, size_t len)
    {
     int ret = 0;
     char *src = _src;
     char *dst = _dst;
     unsigned int ch;
    
     while (*src) {
      if (*src == '\\' && *(src+1) == 'x') {
       sscanf(src + 2, "%2x", &ch);
       src += 4;
       *dst++ = (unsigned char)ch;
      } else {
       *dst++ = *src++;
      }
      ret++;
     }
     return ret;
    }
    
    static void transfer(int fd, uint8_t const *tx, uint8_t const *rx, size_t len)
    {
     int ret;
    
     struct spi_ioc_transfer tr = {
      .tx_buf = (unsigned long)tx,
      .rx_buf = (unsigned long)rx,
      .len = len,
      .delay_usecs = delay,
      .speed_hz = speed,
      .bits_per_word = bits,
     };
    
     if (mode & SPI_TX_QUAD)
      tr.tx_nbits = 4;
     else if (mode & SPI_TX_DUAL)
      tr.tx_nbits = 2;
     if (mode & SPI_RX_QUAD)
      tr.rx_nbits = 4;
     else if (mode & SPI_RX_DUAL)
      tr.rx_nbits = 2;
     if (!(mode & SPI_LOOP)) {
      if (mode & (SPI_TX_QUAD | SPI_TX_DUAL))
       tr.rx_buf = 0;
      else if (mode & (SPI_RX_QUAD | SPI_RX_DUAL))
       tr.tx_buf = 0;
     }
    
     ret = ioctl(fd, SPI_IOC_MESSAGE(1), &tr);
     if (ret < 1)
                    printf(device);
      pabort("can't send spi message");
    
     if (verbose)
      hex_dump(tx, len, 32, "TX");
     hex_dump(rx, len, 32, "RX");
    }
    
    static void print_usage(const char *prog)
    {
     printf("Usage: %s [-DsbdlHOLC3]\n", prog);
     puts("  -D --device   device to use (default /dev/spidev1.1)\n"
          "  -s --speed    max speed (Hz)\n"
          "  -d --delay    delay (usec)\n"
          "  -b --bpw      bits per word \n"
          "  -l --loop     loopback\n"
          "  -H --cpha     clock phase\n"
          "  -O --cpol     clock polarity\n"
          "  -L --lsb      least significant bit first\n"
          "  -C --cs-high  chip select active high\n"
          "  -3 --3wire    SI/SO signals shared\n"
          "  -v --verbose  Verbose (show tx buffer)\n"
          "  -p            Send data (e.g. \"1234\\xde\\xad\")\n"
          "  -N --no-cs    no chip select\n"
          "  -R --ready    slave pulls low to pause\n"
          "  -2 --dual     dual transfer\n"
          "  -4 --quad     quad transfer\n");
     exit(1);
    }
    
    static void parse_opts(int argc, char *argv[])
    {
     while (1) {
      static const struct option lopts[] = {
       { "device",  1, 0, 'D' },
       { "speed",   1, 0, 's' },
       { "delay",   1, 0, 'd' },
       { "bpw",     1, 0, 'b' },
       { "loop",    0, 0, 'l' },
       { "cpha",    0, 0, 'H' },
       { "cpol",    0, 0, 'O' },
       { "lsb",     0, 0, 'L' },
       { "cs-high", 0, 0, 'C' },
       { "3wire",   0, 0, '3' },
       { "no-cs",   0, 0, 'N' },
       { "ready",   0, 0, 'R' },
       { "dual",    0, 0, '2' },
       { "verbose", 0, 0, 'v' },
       { "quad",    0, 0, '4' },
       { NULL, 0, 0, 0 },
      };
      int c;
    
      c = getopt_long(argc, argv, "D:s:d:b:lHOLC3NR24p:v", lopts, NULL);
    
      if (c == -1)
       break;
    
      switch (c) {
      case 'D':
       device = optarg;
       break;
      case 's':
       speed = atoi(optarg);
       break;
      case 'd':
       delay = atoi(optarg);
       break;
      case 'b':
       bits = atoi(optarg);
       break;
      case 'l':
       mode |= SPI_LOOP;
       break;
      case 'H':
       mode |= SPI_CPHA;
       break;
      case 'O':
       mode |= SPI_CPOL;
       break;
      case 'L':
       mode |= SPI_LSB_FIRST;
       break;
      case 'C':
       mode |= SPI_CS_HIGH;
       break;
      case '3':
       mode |= SPI_3WIRE;
       break;
      case 'N':
       mode |= SPI_NO_CS;
       break;
      case 'v':
       verbose = 1;
       break;
      case 'R':
       mode |= SPI_READY;
       break;
      case 'p':
       input_tx = optarg;
       break;
      case '2':
       mode |= SPI_TX_DUAL;
       break;
      case '4':
       mode |= SPI_TX_QUAD;
       break;
      default:
       print_usage(argv[0]);
       break;
      }
     }
     if (mode & SPI_LOOP) {
      if (mode & SPI_TX_DUAL)
       mode |= SPI_RX_DUAL;
      if (mode & SPI_TX_QUAD)
       mode |= SPI_RX_QUAD;
     }
    }
    
    int main(int argc, char *argv[])
    {
     int ret = 0;
     int fd;
     uint8_t *tx;
     uint8_t *rx;
     int size;
    
     parse_opts(argc, argv);
    
     fd = open(device, O_RDWR);
     if (fd < 0)
      pabort("can't open device");
    
     /*
      * spi mode
      */
     ret = ioctl(fd, SPI_IOC_WR_MODE32, &mode);
     if (ret == -1)
      pabort("can't set spi mode");
    
     ret = ioctl(fd, SPI_IOC_RD_MODE32, &mode);
     if (ret == -1)
      pabort("can't get spi mode");
    
     /*
      * bits per word
      */
     ret = ioctl(fd, SPI_IOC_WR_BITS_PER_WORD, &bits);
     if (ret == -1)
      pabort("can't set bits per word");
    
     ret = ioctl(fd, SPI_IOC_RD_BITS_PER_WORD, &bits);
     if (ret == -1)
      pabort("can't get bits per word");
    
     /*
      * max speed hz
      */
     ret = ioctl(fd, SPI_IOC_WR_MAX_SPEED_HZ, &speed);
     if (ret == -1)
      pabort("can't set max speed hz");
    
     ret = ioctl(fd, SPI_IOC_RD_MAX_SPEED_HZ, &speed);
     if (ret == -1)
      pabort("can't get max speed hz");
    
     printf("spi mode: 0x%x\n", mode);
     printf("bits per word: %d\n", bits);
     printf("max speed: %d Hz (%d KHz)\n", speed, speed/1000);
    
     if (input_tx) {
      size = strlen(input_tx+1);
      tx = malloc(size);
      rx = malloc(size);
      size = unescape((char *)tx, input_tx, size);
      transfer(fd, tx, rx, size);
      free(rx);
      free(tx);
     } else {
      transfer(fd, default_tx, default_rx, sizeof(default_tx));
     }
    
     close(fd);
    
     return ret;
    }
    
          
         
        
       
      
     
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • valentino.ricci
    0 valentino.ricci over 9 years ago

    On Microzed: Petalinux 2016.3, linux 4.6 same issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    Hi. I'm running across similar issues (seeing SPI timeout message). Did someone find a solution to this issue ?  The message in the log at /var/log/messages is below: Jan  2 23:26:53 avnet-digilent-zedboard-2017_3 user.err kernel: spidev spi32765.1: SPI transfer timed out
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago
    Issuing multiple 1 byte transactions (as opposed to 1 transaction containing multiple bytes) seems to work without causing SPI timeouts.

    So for example, the code below issues 16 transfers each 1 byte long and work OK:

    #include <stdint.h>
    #include <stdlib.h>
    #include <stdio.h>
    #include <string.h>
    #include <fcntl.h>
    #include <unistd.h>
    #include <sys/ioctl.h>
    #include <linux/types.h>
    #include <linux/spi/spidev.h>

    int fp;
    struct spi_ioc_transfer xfer[16];
    uint8_t tx[16];
    uint8_t rx[16];
    memset(xfer, 0, sizeof xfer); // Initialize data structures to 0
    memset(tx,0,sizeof tx);
    memset(rx, 0, sizeof rx);

    for (i=0;i<16;i++) { tx[i] = 0xA0 + i;} // Bytes to transmit
    for (i=0; i<16; i++) { // setup 16 transfers, each 1 byte long
      xfer[i].speed_hz = 4*1000*1000; // 4Mhz
      xfer[i].bits_per_word = 8;
      xfer[i].tx_buf = (unsigned long)&tx[i]; // tranmision is most significant bit first. If you need least significant bit first, you need to swizzle the tx buffer contents. The LSB_FIRST mode setting in SPIDev doesnt seem to work.
      xfer[i].rx_buf = (unsigned long)&rx[i];
    xfer[i].len = 1; // each transfer is only 1 byte long
    }
    fp = open("/dev/spidev32765.1", O_RDWR); // on my zed board SPI1 showup at node 32765. Also, using chip select 1, since chip select 0 has bug. 
    ioctl(fp, SPI_IOC_MESSAGE(16), xfer); // send the 16 transfers
    close(fp);

     

    The device tree file (in petalinux flow it's at: project-spec/meta-user/recipes-bsp/device-tree/files/system-user.dtsi) needs following added to enable SPI1 using chip select 1:

     

    &spi1 {

        is-decoded-cs = <0>;
       num-cs = <2>;
       status = "okay"; 

       spidev1@0 {

             compatible="spidev";

             reg = <1>; //chipselect

             spi-max-frequency = <5000000>; //5 Mhz

              };
    };


     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello,

    Please ask this question over at Xilinx as it appears to be an issue related to Petalinux.

    Thanks,

    Josh