Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development AMP Zedboard Vivado
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 364 subscribers
  • Views 545 views
  • Users 0 members are here
Related

AMP Zedboard Vivado

e14 Contributor
e14 Contributor over 11 years ago

I am trying to run a simple application where core 0 writes to a shared register and core 1 reads from that register, printing out the value.

I created a custom IP to be the shared register in the FPGA. I've confirmed with one core that I am able to read and write to that register.

However I cannot figure out how to get both of these to run simultaneously. Looking online it seems like I might need to go the route of something like FreeRTOS.

Is there really no way for me to program this within the Xilinx SDK?

All of the examples I have found for AMP are either for Altera tools, ISE, or different boards.

Thanks

edit:
I attempted to create a bootable SD of this using:
FSBL > system.bit > core0.elf > core1.elf

When I don't use the core1.elf to generate the boot.bin the program loads and functions correctly (different functionality than described before - it just writes and reads from a register).

When I use the core1.elf in the boot.bin generation nothing works at all.

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 11 years ago

    Hi Steve,

    The FSBL from Zynq Software SpeedWay training is the same stock FSBL.  The only thing that is special for AMP is making sure that you get the order of the executable files (and the execution memory space) listed correctly in the BOOT.BIN container file.

    As for standalone_amp BSP, there are not really many differences between the stock standalone BSP and the AMP one.  All I did was take a diff of all of the files between the standalone_amp BSP that is provided in XAPP1079 and the stock standalone BSP that comes with Xilinx SDK.  Then I copied the latest stock version of standalone BSP from the Xilinx install folder and make a copy called standalone_amp and merge the differences from the version provided with XAPP1079.  I have done this process twice already, once migrating the SpeedWay labs to 2013.3 tools and again migrating to 2014.4 tools and I didn't have any problems. 

    I am not aware of a more detailed guide than XAPP1079.

    The changes are mostly trivial where some critical processor resources are not reinitialized by the second CPU.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 11 years ago

    Hi Steve,

    The FSBL from Zynq Software SpeedWay training is the same stock FSBL.  The only thing that is special for AMP is making sure that you get the order of the executable files (and the execution memory space) listed correctly in the BOOT.BIN container file.

    As for standalone_amp BSP, there are not really many differences between the stock standalone BSP and the AMP one.  All I did was take a diff of all of the files between the standalone_amp BSP that is provided in XAPP1079 and the stock standalone BSP that comes with Xilinx SDK.  Then I copied the latest stock version of standalone BSP from the Xilinx install folder and make a copy called standalone_amp and merge the differences from the version provided with XAPP1079.  I have done this process twice already, once migrating the SpeedWay labs to 2013.3 tools and again migrating to 2014.4 tools and I didn't have any problems. 

    I am not aware of a more detailed guide than XAPP1079.

    The changes are mostly trivial where some critical processor resources are not reinitialized by the second CPU.

    Regards,

    -Kevin