Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Unresolved inclusion: "xparameters.h"
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 365 subscribers
  • Views 5238 views
  • Users 0 members are here
Related

Unresolved inclusion: "xparameters.h"

y_okada
y_okada over 11 years ago

I have error messages "Unresolved inclusion: xparameters.h" in xsdk.

vivado and xsdk are v2014.4


Followings are what I did:
-----
0. Export hdf from vivado (including bitstream)
1. Launch xsdk
2. File -> New -> BSP (standalone_bsp_0)
-----

Then, when I see the xgpiops_sinit.c file
( standalone_bsp_0/ps7_cortexa9_0/libsrc/gpiops_v2_2/src/xgpiops_sinit.c )
the xsdk says
"Unresolved inclusion: xparameters.h"
for #include "xparameters.h"

However, the xparameters.h does exist as
"standalone_bsp_0/ps7_cortexa9_0/include/xparameters.h".

And the xparameters.h is included as the BSP in xsdk.


Where should I check to avoid this error?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago
    I am running the USB2.0  AXI tutorial on zed board . while launching SDK and adding the source file(s) for bulk_perform application, I am getting error 
     
    'XPAR_INTC_0_USB_0_VEC_ID' undeclared (first use in this function) in xusb_storage.c
    i also add the xparameters.h file in the code. while going through that code I found that 
    #define 'XPAR_INTC_0_USB_0_VEC_ID is not defined in it.
    so kindly let me know the proper solution for this.
     
    this is the Error:
    Description Resource Path Location Type
    'XPAR_INTC_0_USB_0_VEC_ID' undeclared (first use in this function) xusb_storage.c /usb_mass_test/src line 103 C/C++ Problem
     
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago
    I am running the USB2.0  AXI tutorial on zed board . while launching SDK and adding the source file(s) for bulk_perform application, I am getting error 
     
    'XPAR_INTC_0_USB_0_VEC_ID' undeclared (first use in this function) in xusb_storage.c
    i also add the xparameters.h file in the code. while going through that code I found that 
    #define 'XPAR_INTC_0_USB_0_VEC_ID is not defined in it.
    so kindly let me know the proper solution for this.
     
    this is the Error:
    Description Resource Path Location Type
    'XPAR_INTC_0_USB_0_VEC_ID' undeclared (first use in this function) xusb_storage.c /usb_mass_test/src line 103 C/C++ Problem