Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Zedboard & Fmcomms2 QSPI boot and Image
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 363 subscribers
  • Views 940 views
  • Users 0 members are here
Related

Zedboard & Fmcomms2 QSPI boot and Image

e14 Contributor
e14 Contributor over 11 years ago

Hello to all, i have some problem for creating the QSPI image form Sdk Vivado or Sdk 14.4 .

When i create the qspi.msc whit sdk 14_4 the board boot well and the fpga is programed but i have this message out on serial terminal

Copying ramdisk...
Wrong Image Format for bootm command
ERROR: can't get kernel image!
zynq-uboot>

i make the qspi image whit fsbl, fil.bit, u-boot.elf
zImage.bin, devitree and ramdisk image.

I had found the qspi address in zynq.dtsi file on petalinux_2014_r2, i think ... and add this qspi offset in qspi image procedure found on pdf files CTT. When i program the qspi flash the fpga is programmed and the u-boot start
but dont found the kernel image for zImage or uImage format

here the definition of qspi address :


primary_flash: ps7-qspi@0 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "st,m25p80";
reg = <0x0>;
spi-max-frequency = <50000000>;
partition@0x00000000 {
label = "boot";
reg = <0x00000000 0x00500000>;
};
partition@0x00500000 {
label = "bootenv";
reg = <0x00500000 0x00020000>;
};
partition@0x00520000 {
label = "config";
reg = <0x00520000 0x00020000>;
};
partition@0x00540000 {
label = "image";
reg = <0x00540000 0x00a80000>;
};
partition@0x00fc0000 {
label = "spare";
reg = <0x00fc0000 0x00000000>;
};
};

When i try to make the same file whit vivado 2014 the board doesn't boot or program the fpga and the i cant see the blue led done.

where i wrong ?

thanks in advance
-Nicolas

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Ron,
    my target board is ZedBoard and Fmcomms2-EZB, my system enviroment is :

       Virtual Machine Linux Centos and Petalinux 2014_R2
       Vivado 2014 2 and SDK

    Im need to program the Qspi Flash whit a linux boostrap image whitout Sd card

    i will see the PicoZed reference documents

    thankyou in advance

    Nicolas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    OK, let me know if that works for you.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    OK, let me know if that works for you.

    Ron