Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development UltraZed Board : Cannot Debug Linux Application
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 365 subscribers
  • Views 849 views
  • Users 0 members are here
Related

UltraZed Board : Cannot Debug Linux Application

100docjay
100docjay over 9 years ago

I got an ultrazed board.  The provided Linux seems to lack any debugging capability with the SDK.

I noticed that with the original zed board  the following was running on startup (top command in linux):

 

/usr/sbin/tcf-agent -d -L- -l0

 

But this is not present in the supplied ultrazed linux.  Is there any built in way to debug from the SDK with this build or do I have to recompile the kernel to debug anything.

 

This is a big deal for me who is just starting out trying to use the board.  I have no experience and no set up to do kernel development.

  • Sign in to reply
  • Cancel

Top Replies

  • zedhed
    zedhed over 9 years ago +1 verified
    Hi docjay, IIRC, tcf-agaent was removed from the 2016.2 out-of-box image to help decrease boot time to login prompt. So you will have to build you own image with tcf-agent but they can start with the 2017…
Parents
  • zedhed
    0 zedhed over 9 years ago

    Hi docjay,

    IIRC, tcf-agaent was removed from the 2016.2 out-of-box image to help decrease boot time to login prompt.

    So you will have to build you own image with tcf-agent but they can start with the 2017.2 BSP which should help save some time:

    http://ultrazed.org/support/design/17596/131

    You can use that with the Xilinx PetaLinux tools to create a new project based upon the BSP settings and add

    $ petalinux-config -c rootfs

    In fact, @narrucmot just pointed out tcf-agent should already be in the pre-built images that come with the 2017.2 BSP so you might not have to re-build after all:

    #
    # tcf-agent
    #
    CONFIG_tcf-agent=y
    # CONFIG_tcf-agent-dev is not set
    # CONFIG_tcf-agent-dbg is not set

    Best Regards,

    -Kevin

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 9 years ago

    Hi docjay,

    IIRC, tcf-agaent was removed from the 2016.2 out-of-box image to help decrease boot time to login prompt.

    So you will have to build you own image with tcf-agent but they can start with the 2017.2 BSP which should help save some time:

    http://ultrazed.org/support/design/17596/131

    You can use that with the Xilinx PetaLinux tools to create a new project based upon the BSP settings and add

    $ petalinux-config -c rootfs

    In fact, @narrucmot just pointed out tcf-agent should already be in the pre-built images that come with the 2017.2 BSP so you might not have to re-build after all:

    #
    # tcf-agent
    #
    CONFIG_tcf-agent=y
    # CONFIG_tcf-agent-dev is not set
    # CONFIG_tcf-agent-dbg is not set

    Best Regards,

    -Kevin

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer