Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development axi gpio data registers
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 2384 views
  • Users 0 members are here
Related

axi gpio data registers

e14 Contributor
e14 Contributor over 9 years ago

Using xilinx sdk I want to write code in 'C' that will  transfer data from one zedboard to a second zedboard.  I'm doing this via FMC connecter.

I have two separate block diagram in vivado and  each is  setup using a dual channel axi gpio. With gpio width of 32.

I setup my constraint file so that my input and outputs correspond correctly.

In vivado the address editor says I have 64k range.

Offset address 0x4120_0000 High address 0x4120_FFFF

I was hoping to "preload" the axi gpio data register from my "send" 'C' code and "unload" the axi gpio data register from my "receive" 'C' code.

In my "send" 'C' code I write to the axi gpio data register

XGpioPs_WriteReg(XPAR_GPIO_0_BASEADDR,0x8, 0x01234567);

XGpioPs_WriteReg(XPAR_GPIO_0_BASEADDR,0x18, 0x89ABCDEF);

In my "receive" 'C' code I read from the axi gipi data register

Data = XGpioPs_ReadReg(XPAR_GPIO_0_BASEADDR,0x0);

Xil_printf("Addres 0 has data value %x\r\n, Data);

Data = XGpioPs_ReadReg(XPAR_GPIO_0_BASEADDR,0x10);

Xil_printf("Addres 10 has data value %x\r\n, Data);

The result printed to the screen is

Addres 0 has data value 89ABCDEF

Addres 10 has data value 89ABCDEF

 

As you can see the second write statement is writing to both register addresses. 

Why isn't each address retaining it's original assigned data?

Bottom line question is how or where can I preload data on my "send" zedboard preferably using the sdk so that it can me "unloaded" via FMC connecter with my "receive" zedboard preferably also using the sdk.

Thank you for help.

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Cgonzales,

    Your code you reference above seems incorrect. If you refer to the offset register table of AXI GPIO 

    https://www.xilinx.com/support/documentation/ip_documentation/axi_gpio/v2_0/pg144-axi-gpio.pdf

    image

    Based off this you should be writing to channel 1 0x0, then reading from channel 1 0x0 and also writing to channel 2 0x8 and then reading from channel 2 0x8. I am not sure how you are getting 89ABCDEF in both data registers when you are writing it to offset register 0x18.

    --Josh