Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development DStream does not recognize Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 364 subscribers
  • Views 1236 views
  • Users 0 members are here
Related

DStream does not recognize Zedboard

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I would like to use arm ds5 tools to debug my zedboard.

I followed tutorials on this website (http://zedboard.org/reference-designs-categories/debugging-arm-processor-systems-using-arm-ds-5) to try configuring DS-5 for ZED.

So I made hardware connection as indicated in the tutorial one, that is to say connect the ribbon cable and set the jumper correctly. Then the Debug Hardware Configuration of ARM DS5 is not able to autoconfigure my device (tutorial 2), and I get the following message :
"Auto configure failed. Check the debug Hardware connection with the target or try using a lower fixed frequency."

However I am able to recognize the device with a jtag probe from xilinx and with the Vivado Hardware Manager.

Any idea of my problem with my dstream ?

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 11 years ago

    HI Clement,

    I have not tried this recently, but I wanted to first make sure that your board connections are correct.

    Are you using our Processor Debug Adapter (AES-ZBDB-ADPT-G) to connect DSTREAM to ZedBoard's 14-pin (PC4) header at J15?

    http://www.em.avnet.com/en-us/design/drc/Pages/ZedBoard-Processor-Debug-Adapter.aspx

    Some DS-5 customers try to connect their DSTREAM to the Zynq XADC header at J2 which is an incorrect connection.

    Also, to connect to the ARM DAP, I believe that Zynq needs to be configured for cascaded JTAG boot mode(JP7-JP11 set to GND).

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to zedhed

    Yes I am using the Processor Debug Adapter to connect DSTREAM to Zedboard's 14-pin and I do not use the Zynq XADC header. The Jumper JP7 to JP11 are all set to GND.

    Moreover I have tried to use DSTREAM with another Zedboard, thinking some of zedboard part was broken, and I still have the same problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    I used the same settings and hit exactly the same bahavior as you do. This is strange. Is there anyone succeeded in using DS-5 to connect to the Zedboard before?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    I used the same settings and hit exactly the same bahavior as you do. This is strange. Is there anyone succeeded in using DS-5 to connect to the Zedboard before?