Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development How to use DS3231M PMOD
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 364 subscribers
  • Views 899 views
  • Users 0 members are here
Related

How to use DS3231M PMOD

hai.bi
hai.bi over 11 years ago

My ultimate goal is to use an RTC and I have bought DS3231M PMOD so I am going to try it on MicroZed.


I have gone through Vivado and configured I2C0 on 14-15 and exported according to the link http://microzed.org/content/problem-linaro-and-i2c-devices


I am wondering what to do in kernel config?  Since I am using the MIO, what do I need to do for the I2C hardware bus support?  Then what to do with the driver?  there is only DS3232 driver should I use it?


Then should I modify the device tree manually before build?


Regards,

  • Sign in to reply
  • Cancel
Parents
  • hai.bi
    0 hai.bi over 11 years ago

    Thanks to all your comments.  I have reached a deeper level.  I am able to use i2cset 0 0x68 0xD0 to send out commands and see response on the scope.  And I am using the PMOD on the J5 so it's MIO. There was a glitch problem on the MIO i2C but I want to see it's working before I move on to a better eMIO.

    However, when I boot the board, there was no i2c activity (before I use i2cset manually).  The following was taken out of the output:

    i2c /dev entries driver
    cdns-i2c e00004000.i2c: 400 kHz mmio e00004000 irq 57
    ...
    /opt/pkg/.... drivers/rtc/hctosys.c: unable to open rtc device (rtc0)


    So I am thinking there has to be some configuration not right resulting in the Linux not accessing the i2c 0 correctly for rtc0.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • hai.bi
    0 hai.bi over 11 years ago

    Thanks to all your comments.  I have reached a deeper level.  I am able to use i2cset 0 0x68 0xD0 to send out commands and see response on the scope.  And I am using the PMOD on the J5 so it's MIO. There was a glitch problem on the MIO i2C but I want to see it's working before I move on to a better eMIO.

    However, when I boot the board, there was no i2c activity (before I use i2cset manually).  The following was taken out of the output:

    i2c /dev entries driver
    cdns-i2c e00004000.i2c: 400 kHz mmio e00004000 irq 57
    ...
    /opt/pkg/.... drivers/rtc/hctosys.c: unable to open rtc device (rtc0)


    So I am thinking there has to be some configuration not right resulting in the Linux not accessing the i2c 0 correctly for rtc0.