Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development How to use DS3231M PMOD
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 364 subscribers
  • Views 897 views
  • Users 0 members are here
Related

How to use DS3231M PMOD

hai.bi
hai.bi over 11 years ago

My ultimate goal is to use an RTC and I have bought DS3231M PMOD so I am going to try it on MicroZed.


I have gone through Vivado and configured I2C0 on 14-15 and exported according to the link http://microzed.org/content/problem-linaro-and-i2c-devices


I am wondering what to do in kernel config?  Since I am using the MIO, what do I need to do for the I2C hardware bus support?  Then what to do with the driver?  there is only DS3232 driver should I use it?


Then should I modify the device tree manually before build?


Regards,

  • Sign in to reply
  • Cancel
Parents
  • hai.bi
    0 hai.bi over 11 years ago

    I think I have made further:

    I am using the following command to link the rtc with the i2c:

    echo ds3232 0x68 > /sys/class/i2c-adapter/i2c-0/new_device

    Then I can see that the system instantiated device.  So I think it's working.  I was just I didn't know you have to do that under Linux command prompt.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • hai.bi
    0 hai.bi over 11 years ago

    I think I have made further:

    I am using the following command to link the rtc with the i2c:

    echo ds3232 0x68 > /sys/class/i2c-adapter/i2c-0/new_device

    Then I can see that the system instantiated device.  So I think it's working.  I was just I didn't know you have to do that under Linux command prompt.