Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development linux application
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 450 views
  • Users 0 members are here
Related

linux application

e14 Contributor
e14 Contributor over 13 years ago

Good evening,  after build in the linux zedboard. I want to turn the LEDs without the write_led . with a Linux application in the SDK tool:

using the port in the file system.ucf
Net processing_system7_0_GPIO <7> LOC = T22 | IOSTANDARD = LVCMOS33;
Net processing_system7_0_GPIO <8> LOC = T21 | IOSTANDARD = LVCMOS33;
Net processing_system7_0_GPIO <9> LOC = U22 | = IOSTANDARD= LVCMOS33;
Net processing_system7_0_GPIO <10> LOC = U21 | = IOSTANDARD =LVCMOS33;
Net processing_system7_0_GPIO <11> LOC = V22 | = IOSTANDARD =LVCMOS33;
Net processing_system7_0_GPIO <12> LOC = W22 | IOSTANDARD = LVCMOS33;
Net processing_system7_0_GPIO <13> LOC = U19 | = IOSTANDARD =LVCMOS33;
Net processing_system7_0_GPIO <14> LOC = U14 | = IOSTANDARD= LVCMOS33;

I don't no if the port using is correct or not?



# include "xgpio.h"
# include "xparameters.h"
int main ();
{
xgpio LED;

XGpio_Initialize (& led, XPAR_PS7_GPIO_0_DEVICE_ID);
XGpio_SetDataDirection (& LED,1,x0000)//i can find the right mask derection Bits 7-14
XGpio_DiscreteWrite (& LED,1,0xffff);

return 0;
}

thank you :)

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Linux supports user space gpio through reads and writes to special files. You don't have to write a special driver. Google on Linux GPIO.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • eactor
    0 eactor over 13 years ago

    It's also part of the Avnet Speedway Training "mplementing Linux on the Zynq-7000 SoC" and discussed in:
    -Chapter-3.1 tLinux Device Drivers tView
    -Lab-3.1 Device Drivers and MIO GPIO Hardware

    cheers eactor

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    @eactor, @mikewhy: thank you for your help :)