Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Connecting USB devices to Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 362 subscribers
  • Views 298 views
  • Users 0 members are here
Related

Connecting USB devices to Zedboard

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I would like to access standard USB devices (flash drives or mouse) from my zedboard running Linux (the Xilinx version).
I activated the option in the Linux kernel configuration and checked that the "ds-mode in the Device Tree is set to "host". I also connected jumper JP3 to be in "host mode".

But when I plug anything in the Usb OTG port, nothing happens. The only message I get from USB is during startup, where it seems to go into sleep mode.
How can I get it to work?

Thanks,

Michele

PS: my startup messages

root@zynq:~# dmesg | grep usb
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
xusbps-ehci xusbps-ehci.0: Xilinx PS USB EHCI Host Controller
xusbps-ehci xusbps-ehci.0: new USB bus registered, assigned bus number 1
xusbps-ehci xusbps-ehci.0: reset hcs_params 0x10011 dbg=0 ind cc=0 pcc=0 ordered ports=1
xusbps-ehci xusbps-ehci.0: reset hcc_params 0006 thresh 0 uframes 256/512/1024 park
xusbps-ehci xusbps-ehci.0: park 0
xusbps-ehci xusbps-ehci.0: reset command 0080002 (park)=0 ithresh=8 period=1024 Reset HALT
xusbps-ehci xusbps-ehci.0: ...powerdown ports...
xusbps-ehci xusbps-ehci.0: irq 53, io mem 0x00000000
xusbps-ehci xusbps-ehci.0: init command 0010005 (park)=0 ithresh=1 period=512 RUN
xusbps-ehci xusbps-ehci.0: USB 2.0 started, EHCI 1.00
usb usb1: default language 0x0409
usb usb1: udev 1, busnum 1, minor = 0
usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: Xilinx PS USB EHCI Host Controller
usb usb1: Manufacturer: Linux 3.12.0-xilinx-dirty ehci_hcd
usb usb1: SerialNumber: xusbps-ehci.0
usb usb1: usb_probe_device
usb usb1: configuration #1 chosen from 1 choice
usb usb1: adding 1-0:1.0 (config #1, interface 0)
hub 1-0:1.0: usb_probe_interface
hub 1-0:1.0: usb_probe_interface - got id
usbcore: registered new interface driver usbserial
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usb usb1: bus auto-suspend, wakeup 1
xusbps-ehci xusbps-ehci.0: suspend root hub