Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Linux Driver to manage Interrupt sent from PL
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 363 subscribers
  • Views 736 views
  • Users 0 members are here
Related

Linux Driver to manage Interrupt sent from PL

e14 Contributor
e14 Contributor over 13 years ago

Hello everybody,

I'm working on writing a linux driver able to detect an interrupt coming from PL. This is what I've done:

1) added an AXI Timer in XPS and interconnected its interrupt output to GIC on PS.

2) modyfied DTS by adding:

axi_timer_0: axitimer@42800000 {
tttcompatible = "xlnx,axi-timer";
tttreg = <0x42800000 0x10000>;
tttinterrupts = <0x0 0x37 0x0>;
tttinterrupt-parent = <&gic>;
tt};

3) wrote a linux kernel module able to detect the component declared in the DTS. I'm pretty sure this works fine as I'm able to read the address and, most important in my opinion, the irq number. The module is correctly added to the running kernel of the zedboard by typing: insmod timer_module.ko

4) I wrote a simple software that programs the timer and enables it. Unfortunately it seems like the gic isn't able to detect the interrupt request coming from the timer itself.

Do I miss something?

thank you!

sticken

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Linux kernel module correctly sees 0x37 as 87: I printed it using printk(). Number 87 came from XPS, then I subtracted 32 (read this somewhere) and converted the result to hex notation.

    Do I have to configure something about the GIC or the Cortex-A9

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Linux kernel module correctly sees 0x37 as 87: I printed it using printk(). Number 87 came from XPS, then I subtracted 32 (read this somewhere) and converted the result to hex notation.

    Do I have to configure something about the GIC or the Cortex-A9