Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development U boot bad characters
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 498 views
  • Users 0 members are here
Related

U boot bad characters

e14 Contributor
e14 Contributor over 11 years ago

Hello all,
I have compiled U-boot for zynq_zed board and create an fsbl and also add bitstream and add the Uboot.elf
the fsbl is runnig and giving correct bytes on the Terminal but the uboot is out of baudrate and giving lot of garabage. I checked the baudrate in Uboot (zynq_common.h) it is correct , and I also tried to change Uart clock to 50 mhz but it also didnt work.
Please any idea ?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    U-boot typically is a pretty straightforward standalone program to get running, once it has been correctly configured (and the defaults in the hierarchy for ZedBoard typically do that fine).  The default is to run at 115,200 - is that the rate you are selecting in your serial program?  Have you verified that you can receive output using a simple standalone program that you can auto-generate from the SDK, such as HelloWorld (but any of the application templates will work).

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Yes for sure standalone from SDK give correct data I also downloaded an fsbl.elf file from net and I gave good result with U-boot but my fsbl which is working with standalone App is not working with U-boot