Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Interrupt Handler in Kernel Module
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 365 subscribers
  • Views 2067 views
  • Users 0 members are here
Related

Interrupt Handler in Kernel Module

e14 Contributor
e14 Contributor over 13 years ago

Does anyone have a working linux device driver that works for interrupt of custom ip-cores?

The AR 51138 shows an example ip-core that contains an own interrupt controller that supports multiple interrupt sources and registers into the global interrupt controller of the Zynq. But the example software is only bare-metal not linux.

http://www.xilinx.com/support/answers/51138.htm

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    A short while ago i did the same. this is the thread i used to gather infrmation:
    http://forums.xilinx.com/t5/Embedded-Linux/AR-50572-Axi-timer-interrupts-in-linux/td-p/335077

    The driver i posted there is able to start on its own, but you can use a script/application to write&read.
    it stops after 100 interrupts, so you might need/want to change that too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cdiscepo
    0 cdiscepo over 9 years ago in reply to e14 Contributor

    Hi Brogath,

      I'm able to build, compile, generate my custom kernel module on my Ubuntu machine but when I port the code/Makefile to my Zynq board it can't locate linux system headers (and folder structure)  it would normally expect to find in /lib/modules/4.1.33-pulsar-standard.

    Any ideas where I can get the toolchain/dev kit from to generate my kernel module?  If it can be done locally on the Zynq great but I don't mind cross-compiling from my Ubuntu system

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • cdiscepo
    0 cdiscepo over 9 years ago in reply to e14 Contributor

    Hi Brogath,

      I'm able to build, compile, generate my custom kernel module on my Ubuntu machine but when I port the code/Makefile to my Zynq board it can't locate linux system headers (and folder structure)  it would normally expect to find in /lib/modules/4.1.33-pulsar-standard.

    Any ideas where I can get the toolchain/dev kit from to generate my kernel module?  If it can be done locally on the Zynq great but I don't mind cross-compiling from my Ubuntu system

     

    Thanks