Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development standalone SD card SDIO
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 19 replies
  • Subscribers 357 subscribers
  • Views 3079 views
  • Users 0 members are here
Related

standalone SD card SDIO

Former Member
Former Member over 11 years ago

Hello,

I try to use the SD card of the Zedboard via the SDIO port. I use chans FatFs. First I implemented the diskio.c by my own, but then debugging it I found that there is an implementation in an example project, so now I use that one.
It can be found here:
XilinxSDK2014.2dataembeddedswlibsw_servicesxilffs_v2_1


Initialization works partly, but not fully:
.

XSdPs_SdCardInitialize
XSdPs_Change_ClkFreq(&SdInstance, SD_CLK_25_MHZ);
and XSdPs_Select_Card
.

work propperly, but XSdPs_Get_BusWidth does not anymore.
It seems like commands are accepted, but DMA transfers are not:
.
/*
* Send block write command
*/
Status = XSdPs_CmdTransfer(InstancePtr, CMD55,
tttInstancePtr->RelCardAddr, 0);
tif (Status != XST_SUCCESS) {
t....Status = XST_FAILURE;
t....goto RETURN_PATH;
t}

tBlkCnt = XSDPS_SCR_BLKCNT;
tBlkSize = XSDPS_SCR_BLKSIZE;

t/*
t * Set block size to the value passed
t */
tBlkSize &= XSDPS_BLK_SIZE_MASK;
tXSdPs_WriteReg16(InstancePtr->Config.BaseAddress,
tttXSDPS_BLK_SIZE_OFFSET, BlkSize);

tXSdPs_SetupADMA2DescTbl(InstancePtr, BlkCnt, SCR);

tXSdPs_WriteReg16(InstancePtr->Config.BaseAddress,
tttXSDPS_XFER_MODE_OFFSET,
tttXSDPS_TM_DAT_DIR_SEL_MASK | XSDPS_TM_DMA_EN_MASK);

tStatus = XSdPs_CmdTransfer(InstancePtr, ACMD51, 0, BlkCnt);
tif (Status != XST_SUCCESS) {
t....Status = XST_FAILURE;
t....goto RETURN_PATH;
t}
.
SdPs_CmdTransfer(InstancePtr, ACMD51, 0, BlkCnt) returns with 1.
.

Maybe I did something wrong in the hardware design. I added the SD 0 Peripheral and assigned CD to MIO 47, WP to MIO46.
Do I have to activate the DMA somehow?
.
There is one funny fact: when I let the example program run, a file is generated on the SD, but it cannot be neither read nor written by the zynq.
.
Best regards,
Yaro

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 10 years ago

    You can find a detailed article on using the SD card of the Zedboard (Zynq7000) in standalone software platform on this article: http://embeddedcentric.com/data-logging-using-sd-cards/

    The article also talks about the FatFs APIs, SD card electrical interface, time stamping. Source code and complete Vivado project is included (Vivado Suite 15.2)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 10 years ago

    You can find a detailed article on using the SD card of the Zedboard (Zynq7000) in standalone software platform on this article: http://embeddedcentric.com/data-logging-using-sd-cards/

    The article also talks about the FatFs APIs, SD card electrical interface, time stamping. Source code and complete Vivado project is included (Vivado Suite 15.2)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data