Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Linux kernel does not boot  successfully when reset, only on board power cycle.
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 364 subscribers
  • Views 1990 views
  • Users 0 members are here
Related

Linux kernel does not boot  successfully when reset, only on board power cycle.

e14 Contributor
e14 Contributor over 14 years ago

Hello,

If the board is power cycled, it boots the kernel successfully.

If then the PS-RST button is hit, u-boot loads and starts kernel, but it does not boot successfully.

It seems that the CPU is not reset properly by reset, only by power cycle.

I tried to debug down this and it turns out that the boot stops in the xilinx_dma.c:xilinx_dma_reset(). If I comment out its body, the booting continues further, but it again stops in i2c-xiic.c:xiic_reinit(). Again if body commented out booting continues, but stop later. Here I stopped debugging.

Has anybody experienced such behavior pushing the reset button?

Are there any suggestions or explanations (kernel bug, chip bug, etc.)?

P.S. for the test I build and test the Digilent kernel source three.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Here is the official Digilent statement:
    Hi, Tito,

    The PS-RST button on ZedBoard not only resets the PS system,
    But clears the hardware design in PL system as well.
    Unfortunately the bit file won't get loaded automatically after the reset.

    As a result, the kernel hangs because it is supposed to access some peripheral implemented in PL.

    So, I regret to say that, at this moment, we can only reset the board with the board power switch.

    We will figure some way to walk around the issue in the future.
    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Here is the official Digilent statement:
    Hi, Tito,

    The PS-RST button on ZedBoard not only resets the PS system,
    But clears the hardware design in PL system as well.
    Unfortunately the bit file won't get loaded automatically after the reset.

    As a result, the kernel hangs because it is supposed to access some peripheral implemented in PL.

    So, I regret to say that, at this moment, we can only reset the board with the board power switch.

    We will figure some way to walk around the issue in the future.
    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    The solution here would be to recompile the Kernel and then load in the bit file upon successful boot, and then insmod any drivers needed to communicate to the PL.

    The flow is going to be different for the pre-build linux binary take comes with the Zedboard.

    So to recap, if you final design you would:

    Boot vanilla kernel
    Load PL
    Load drivers into Kernel
    Execute custom code

    Hope that helps to explain things.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    s/Load PS/Load PL/
    I think...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    jsgray, you re correct.  I corrected it in my previous post.  Thanks for pointing that out!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • armfoxy
    0 armfoxy over 12 years ago in reply to e14 Contributor

    Is that problem solved now?


    Many thanks and greetings
    Zynqfan